This is an old revision of the document!
In any transmitter (or receiver) design, frequency stability is of critical importance. Many are interested in both long-term and short-term stability. Long-term frequency stability is concerned with how the output signal varies over a long period of time (minutes, hours, days, or months). It is usually specified as the ratio, Δf/f for a given period of time, expressed as a percentage or in dB. These changes can be the results of thermal, aging, or voltage variations.
Short-term stability, on the other hand, is concerned with variations that occur over a period of seconds or less. These variations can be random or periodic, and are normally referred to a phase noise, measured in dBc/Hz.
The phase noise spectrum of an oscillator shows the noise power in a 1 Hz bandwidth as a function of frequency. Phase noise is defined as the ratio of the noise in a 1 Hz bandwidth at a specified frequency offset, fm, to the oscillator signal amplitude at frequency fo. It is customary to characterize an oscillator in terms of its single-sideband phase noise, where the phase noise in dBc/Hz is plotted as a function of frequency offset, fm, with the frequency axis on a log scale.
Note the curve is approximated by a number of regions, each having a slope of 1/fX, where x = 0 corresponds to the “white” phase noise region (slope = 0dB/decade), and x = 1, corresponds to the “flicker” phase noise region (slope = –20 dB/decade). There are also regions where x = 2, 3, 4, and these regions occur progressively closer to the carrier frequency.
In modern communications algorithms, the phase noise is much more important than frequency stability, as carrier offset and timing correction algorithms will eliminate most frequency accuracy/stability issues.
There are a few great tutorials and writeups includeing: