This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:pluto:users:non_quad [25 Jul 2019 22:59] – Small tweaks Travis Collins | university:tools:pluto:users:non_quad [01 Feb 2021 14:47] (current) – Iulia Moldovan | ||
---|---|---|---|
Line 45: | Line 45: | ||
Receiving is where things can be more complicated. Most (all) integrated transceivers include some sort of Quadrature tracking corrections which try to ensure the signals are correct, and any imperfections in the chip or external circuitry (balun, non-differential traces, etc) are removed. | Receiving is where things can be more complicated. Most (all) integrated transceivers include some sort of Quadrature tracking corrections which try to ensure the signals are correct, and any imperfections in the chip or external circuitry (balun, non-differential traces, etc) are removed. | ||
- | While the frequency domain plot does look close to the same, but we can see that the amplitude is jumping up and down by a few dB. (which is impossible to show in a static picture like this). | + | While the frequency domain plot looks the same, we can see that the amplitude is jumping up and down by a few dB (which is impossible to show in a static picture like this). |
^ Analog Loopback, Frequency Domain, ACG On, Quadrature tracking On ^ | ^ Analog Loopback, Frequency Domain, ACG On, Quadrature tracking On ^ | ||
| {{: | | {{: | ||
- | Its easier to look at this in the time domain. Here the amplitude difference between I & Q is random based on the random difference between the phase of the Rx and Tx PLL. This is indeed completely random and will change any time either PLL settings are touched. Moving one LO to a different setting, and back again, will change this phase offset (which manifest itself as a magnitude difference between I and Q). | + | It' |
^ Analog Loopback, Time Domain, I & Q Data, ACG On, Quadrature tracking On | ^ Analog Loopback, Time Domain, I & Q Data, ACG On, Quadrature tracking On | ||
| {{: | | {{: | ||
- | You can change this magnitude difference digitally by post-processing the sampled data, by using the Phase Rotation control in IIO oscilloscope. It doesn' | + | You can change this magnitude difference digitally by post-processing the sampled data, by using the Phase Rotation control in IIO oscilloscope. It doesn' |
^ Analog Loopback, Time Domain, I & Q Data ^ | ^ Analog Loopback, Time Domain, I & Q Data ^ | ||
Line 143: | Line 143: | ||
For those using a National Instruments USRP Radio, this can be controlled via '' | For those using a National Instruments USRP Radio, this can be controlled via '' | ||
+ | ===== SDRangel ===== | ||
+ | |||
+ | [[https:// | ||
+ | |||
+ | {{: | ||
+ | |||
+ | * '' | ||
+ | * '' | ||
+ | * '' | ||
===== Scope ===== | ===== Scope ===== | ||
This issue will exist on all integrated devices which have some sort of Quadrature tracking feature, including all hardware based on ADI and [[https:// | This issue will exist on all integrated devices which have some sort of Quadrature tracking feature, including all hardware based on ADI and [[https:// |