Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision |
university:tools:pluto:users:name [21 Jan 2021 13:30] – fix link Robin Getz | university:tools:pluto:users:name [08 Feb 2021 15:28] – Change broken link Iulia Moldovan |
---|
==== Tuning Range ==== | ==== Tuning Range ==== |
| |
The tuning range of the [[adi>AD9363]] found inside the PlutoSDR is specified by LO center frequencies between 325 and 3800 MHz. While this is more than a decade of tuning range, and does cover many interesting bands in the [[https://www.ntia.doc.gov/files/ntia/publications/january_2016_spectrum_wall_chart.pdf|US]], [[http://www.erodocdb.dk/docs/doc98/official/pdf/ERCRep025.pdf|Europe]], [[http://www.acma.gov.au/webwr/radcomm/frequency_planning/spectrum_plan/aust_rf_spectrum_plan.doc|Australia]], [[http://www.wpc.dot.gov.in/DocFiles/Book.pdf|India]], [[http://www.tele.soumu.go.jp/e/adm/freq/search/share/plan.htm|Japan]] it's not quite as broad as the [[adi>AD9361]] or [[adi>AD9364]] which has a tuning range of 70 to 6000 MHz, nearly two decades! | The tuning range of the [[adi>AD9363]] found inside the PlutoSDR is specified by LO center frequencies between 325 and 3800 MHz. While this is more than a decade of tuning range, and does cover many interesting bands in the [[https://www.ntia.doc.gov/files/ntia/publications/january_2016_spectrum_wall_chart.pdf|US]], [[http://www.erodocdb.dk/docs/doc98/official/pdf/ERCRep025.pdf|Europe]], [[http://www.acma.gov.au/webwr/radcomm/frequency_planning/spectrum_plan/aust_rf_spectrum_plan.doc|Australia]], [[http://www.tele.soumu.go.jp/e/adm/freq/search/share/plan.htm|Japan]] it's not quite as broad as the [[adi>AD9361]] or [[adi>AD9364]] which has a tuning range of 70 to 6000 MHz, nearly two decades! |
| |
This can easily be overcome by swapping the AD9363 to the AD9364 or the AD9361, as the pinouts of the devices are nearly identical, but it will impact cost. Some users have noted success in [[./customizing#updating_to_the_ad9364|telling the PlutoSDR]] it has a AD9364 inside, which seems to work. | This can easily be overcome by swapping the AD9363 to the AD9364 or the AD9361, as the pinouts of the devices are nearly identical, but it will impact cost. Some users have noted success in [[./customizing#updating_to_the_ad9364|telling the PlutoSDR]] it has a AD9364 inside, which seems to work. |