This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:pluto:usb_otg_host_function_support [05 Jul 2017 11:43] – [Supported WIFI chipsets] Michael Hennerich | university:tools:pluto:usb_otg_host_function_support [27 Jan 2021 22:37] (current) – use wp> interwiki links Robin Getz | ||
---|---|---|---|
Line 2: | Line 2: | ||
| | ||
When the device is powered from the Auxiliary Power Supply it support various HOST functions, such as USB WIFI, Storage and HID. | When the device is powered from the Auxiliary Power Supply it support various HOST functions, such as USB WIFI, Storage and HID. | ||
- | Using the correct cables is the key to [[https:// | + | Using the correct cables is the key to [[wp>USB_On-The-Go|OTG]] operation. |
===== USB Wifi Support ===== | ===== USB Wifi Support ===== | ||
Line 24: | Line 24: | ||
Many cheap and widely available modules will work - If you need a recommendation. The models listed below have been tested: | Many cheap and widely available modules will work - If you need a recommendation. The models listed below have been tested: | ||
* TP-Link TL-WN725N Nano WLAN | * TP-Link TL-WN725N Nano WLAN | ||
+ | * Cisco WUSB600N V2 | ||
===== USB Wired Ethernet Support ===== | ===== USB Wired Ethernet Support ===== | ||
Line 47: | Line 48: | ||
===== Mass Storage Drive Support ===== | ===== Mass Storage Drive Support ===== | ||
- | PlutoSDR or M2k allows in [[https:// | + | PlutoSDR or M2k allows in [[wp>USB_On-The-Go|OTG]] Host mode the attachment of USB Mass Storage Devices. |
- | The supported file system is currently [[https:// | + | The supported file system is currently [[wp>File_Allocation_Table|FAT/ |
Someone may ask what’s the purpose of the USB Mass Storage Device Support? | Someone may ask what’s the purpose of the USB Mass Storage Device Support? | ||
Line 54: | Line 55: | ||
==== Auto Run Support ==== | ==== Auto Run Support ==== | ||
- | After mounting the attached storage the filesystem root is scanned for files named '' | + | After mounting the attached storage the filesystem root is scanned for files named '' |