This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:tools:pluto:usb_otg_host_function_support [05 Jul 2017 11:41] – [Wired USB Ethernet Support] Michael Hennerich | university:tools:pluto:usb_otg_host_function_support [19 Aug 2019 19:49] – [Mass Storage Drive Support] Robin Getz | ||
---|---|---|---|
Line 24: | Line 24: | ||
Many cheap and widely available modules will work - If you need a recommendation. The models listed below have been tested: | Many cheap and widely available modules will work - If you need a recommendation. The models listed below have been tested: | ||
* TP-Link TL-WN725N Nano WLAN | * TP-Link TL-WN725N Nano WLAN | ||
+ | * Cisco WUSB600N V2 | ||
- | ==== Wired USB Ethernet Support ==== | + | ===== USB Wired Ethernet Support |
- | If you want to integrate the PlutoSDR or M2k into a wired Ethernet network directly, without PC in between. Use a wired USB Ethernet | + | If you want to integrate the PlutoSDR or M2k into a wired Ethernet network directly, without PC in between. Use a wired USB Ethernet |
- | Even though the USB support on PlutoSDR or M2k is only USB 2.0 HIGH SPEED. It’s still beneficial to purchase a USB 3.0 Gigabit Ethernet | + | Even though the USB support on PlutoSDR or M2k is only USB 2.0 HIGH SPEED. It’s still beneficial to purchase a USB 3.0 Gigabit Ethernet |
- | Using those USB 3.0 Gigabit Ethernet | + | Using those USB 3.0 Gigabit Ethernet |
Supported chipsets: | Supported chipsets: | ||
Line 48: | Line 49: | ||
PlutoSDR or M2k allows in [[https:// | PlutoSDR or M2k allows in [[https:// | ||
- | The supported file system is currently [[https:// | + | The supported file system is currently [[https:// |
Someone may ask what’s the purpose of the USB Mass Storage Device Support? | Someone may ask what’s the purpose of the USB Mass Storage Device Support? | ||
Line 54: | Line 55: | ||
==== Auto Run Support ==== | ==== Auto Run Support ==== | ||
- | After mounting the attached storage the filesystem root is scanned for files named '' | + | After mounting the attached storage the filesystem root is scanned for files named '' |