This is an old revision of the document!
Everyone has sung to a song on the radio, and it sounds great, as long as the radio is loud enough to drown out your terrible voice (or is that just me?). This is a phenomena known as self reception - when the signal you want to receive is being over loaded by something else.
The ADALM-PLUTO can do this to if you are not careful. The device will have Tx LO Leakage, and the receiver will pick that up, and may swamp out the signal you desire to actually receive.
It's easy to see this with offset tuning. Here is the ADALM-PLUTO with the Rx set to 2400 MHZ, and the Tx set to 2402 MHz, with the internal DDS, set to 3 MHz, and -30dB down (which would put things at 2405 MHz), with the default antennas connected, and the LTE20 Filters loaded.
This shows the peak at the signal (at 2405 MHz, where we expect it), and a LO leakage at 2402 MHz. It's difficult to see what this really means in terms of signal power, so we can look at the actual gain is set to by the Automatic Gain Control (ACG), and the Receive Signal Strength Indicator (RSSI).
We can see the RSSI is 66.25 dB, and the Hardware Gain is set to 43 dB.
If we simply disable the DSS, this is what we see:
Now our RSSI has gone to 90.5 dB and the hardware gain is set to 68 dB (which is still not at the max gain of the device), we are listening to ourselves, not the actual RF.
If we power down the Tx LO with (0
is on, 1
is powerdown):
# iio_attr -c ad9361-phy TX_LO powerdown 1 dev 'ad9361-phy', channel 'altvoltage1' (output), id 'TX_LO', attr 'powerdown', value '0' wrote 2 bytes to powerdown dev 'ad9361-phy', channel 'altvoltage1' (output), id 'TX_LO', attr 'powerdown', value '1'
Then we get:
If we shift things around a bit - if we configure things for a LTE10 signal, (LTE10 filter, with an LTE 10 signal going out the DAC at full scale), and set the Tx and Rx to the same (2400), we can see this:
by offsetting things in 10 MHz steps, how far do things need to be away, so that it stops effecting the receiver.
offset | 0 MHz | 10 MHz | 20 MHz | 30 MHz | 40 MHz | 50 MHz | 60 MHz |
---|---|---|---|---|---|---|---|
RSSI | 48.50 dB | 86.75 dB | 105.00 dB | 112.75 dB | 116.75 dB | 117.00 dB | 117.5 dB |
ACG Gain | 25 dB | 32 dB | 59 dB | 62 dB | 67 dB | 69 dB | 71 dB |
This doesn't mean that you can't transmit/receive on adjacent channels, it just means that the receiver noise floor will not be higher and therefore the receiver will not appear as sensitive when you are doing this.
If you aren't using the transmitter - turn it off, your receiver noise floor will decrease, increasing your receive sensitivity, allowing you to pick up smaller signals from the air.
Test Case | RSSI | AGC Setting |
---|---|---|
Tx On, with Signal | 66.25 dB | 43 dB |
Tx On, without signal | 90.50 dB | 68 dB |
Tx Off | 113.75 dB | 71 dB |