This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:tools:pluto:controlling_the_transceiver_and_transferring_data [28 Apr 2017 16:06] – [Receiving data] Michael Hennerich | university:tools:pluto:controlling_the_transceiver_and_transferring_data [28 Apr 2017 16:29] – [Controlling the transceiver] Michael Hennerich | ||
---|---|---|---|
Line 22: | Line 22: | ||
It shows how to control the AD936x transceiver via a remote connection. | It shows how to control the AD936x transceiver via a remote connection. | ||
- | - Create IIO IP Network context. Instead of ip: | + | - Create IIO IP Network context. Instead of '' |
- Get the AD936x PHY device structure | - Get the AD936x PHY device structure | ||
- Set the TX LO frequency (see [[resources: | - Set the TX LO frequency (see [[resources: | ||
Line 29: | Line 29: | ||
\\ | \\ | ||
<code c> | <code c> | ||
+ | #include < | ||
+ | |||
int main (int argc, char **argv) | int main (int argc, char **argv) | ||
{ | { | ||
Line 46: | Line 48: | ||
iio_device_find_channel(phy, | iio_device_find_channel(phy, | ||
" | " | ||
- | 50000000); /* RX baseband rate 50 MSPS */ | + | 5000000); /* RX baseband rate 5 MSPS */ |
receive(ctx); | receive(ctx); |