This is an old revision of the document!
michael@HAL9000:~/devel$ grep -R “set REQUIRED_VIVADO_VERSION” m2k-fw/hdl/projects/scripts/adi_project.tcl set REQUIRED_VIVADO_VERSION "2016.4" michael@HAL9000:~/devel$
After installing the Xilinx tools, you need to make sure that you have the 32-bit libraries (the Xilinx tools are distributed as 32-bit binaries).
This specifies any shell prompt running on your Linux development host
michael@HAL9000:~/devel$ dpkg --add-architecture i386 michael@HAL9000:~/devel$ apt-get update michael@HAL9000:~/devel$ sudo apt-get install libc6:i386 libstdc++6:i386
There are a few other tools that are necessary in order to build your own Firmware Image.
This specifies any shell prompt running on your Linux development host
michael@HAL9000:~/devel$ sudo apt-get install git build-essential ccache device-tree-compiler dfu-util fakeroot help2man libncurses5-dev libssl1.0-dev mtools rsync u-boot-tools
Starting the build process is just a matter of typing make
within the firmware repository.
The Makefile requires a few environmental variables being set, and of course the ARM GCC toolchain in the PATH.
Some paths maybe adjusted to match your Xilinx Vivado and SDK install folders.
This specifies any shell prompt running on your Linux development host
michael@HAL9000:~/devel$ cd plutosdr-fw or m2k-fw michael@HAL9000:~/devel/plutosdr-fw$ export CROSS_COMPILE=arm-xilinx-linux-gnueabi- michael@HAL9000:~/devel/plutosdr-fw$ export PATH=$PATH:/opt/Xilinx/SDK/2016.2/gnu/arm/lin/bin michael@HAL9000:~/devel/plutosdr-fw$ export VIVADO_SETTINGS=/opt/Xilinx/Vivado/2016.2/settings64.sh michael@HAL9000:~/devel/plutosdr-fw$ make
The initial build takes some time to complete, and also requires an INTERNET connection, since buildroot downloads the source packages from the WEB.
This specifies any shell prompt running on your Linux development host
michael@HAL9000:~/devel/plutosdr-fw$ ls -AGhl build total 52M -rw-rw-r-- 1 michael 69 Apr 19 17:45 boot.bif -rw-rw-r-- 1 michael 446K Apr 19 17:45 boot.bin -rw-rw-r-- 1 michael 446K Apr 19 17:45 boot.dfu -rw-rw-r-- 1 michael 575K Apr 19 17:45 boot.frm -rw-rw-r-- 1 michael 8,3M Apr 19 17:45 pluto.dfu -rw-rw-r-- 1 michael 8,3M Apr 19 17:45 pluto.frm -rw-rw-r-- 1 michael 33 Apr 19 17:45 pluto.frm.md5 -rw-rw-r-- 1 michael 8,3M Apr 19 17:45 pluto.itb -rw-rw-r-- 1 michael 16M Apr 19 17:45 plutosdr-fw-v0.20.zip -rw-rw-r-- 1 michael 471K Apr 19 17:45 plutosdr-jtag-bootstrap-v0.20.zip -rw-r--r-- 1 michael 4,2M Apr 19 17:39 rootfs.cpio.gz drwxrwxr-x 6 michael 4,0K Apr 19 17:45 sdk -rw-rw-r-- 1 michael 940K Apr 19 17:45 system_top.bit -rw-rw-r-- 1 michael 362K Apr 19 17:45 system_top.hdf -rwxrwxr-x 1 michael 409K Apr 19 17:45 u-boot.elf -rw-rw---- 1 michael 128K Apr 19 17:45 uboot-env.bin -rw-rw---- 1 michael 129K Apr 19 17:45 uboot-env.dfu -rw-rw-r-- 1 michael 4,6K Apr 19 17:45 uboot-env.txt -rwxrwxr-x 1 michael 3,2M Apr 19 17:33 zImage -rw-rw-r-- 1 michael 16K Apr 19 17:39 zynq-pluto-sdr.dtb -rw-rw-r-- 1 michael 16K Apr 19 17:39 zynq-pluto-sdr-revb.dtb
File | Comment |
---|---|
pluto.frm | Main PlutoSDR firmware file used with the USB Mass Storage Device |
pluto.dfu | Main PlutoSDR firmware file used in DFU mode |
boot.frm | First and Second Stage Bootloader (u-boot + fsbl + uEnv) used with the USB Mass Storage Device |
boot.dfu | First and Second Stage Bootloader (u-boot + fsbl) used in DFU mode |
uboot-env.dfu | u-boot default environment used in DFU mode |
plutosdr-fw-vX.XX.zip | ZIP archive containg all of the files above |
plutosdr-jtag-bootstrap-vX.XX.zip | ZIP archive containg u-boot and Vivao TCL used for JATG bootstrapping |
File | Comment |
---|---|
boot.bif | Boot Image Format file used to generate the Boot Image |
boot.bin | Final Boot Image |
pluto.frm.md5 | md5sum of the pluto.frm file |
pluto.itb | u-boot Flattened Image Tree |
rootfs.cpio.gz | The Root Filesystem archive |
sdk | Vivado/XSDK Build folder including the FSBL |
system_top.bit | FPGA Bitstream (from HDF) |
system_top.hdf | FPGA Hardware Description File exported by Vivado |
u-boot.elf | u-boot ELF Binary |
uboot-env.bin | u-boot default environment in binary format created form uboot-env.txt |
uboot-env.txt | u-boot default environment in human readable text format |
zImage | Compressed Linux Kernel Image |
zynq-pluto-sdr.dtb | Device Tree Blob for Rev.A |
zynq-pluto-sdr-revb.dtb | Device Tree Blob for Rev.B |
Function | File |
---|---|
PlutoSDR Linux Kernel Config | zynq_pluto_defconfig |
make -C linux ARCH=arm zynq_pluto_defconfig make -C linux -j 8 ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- zImage UIMAGE_LOADADDR=0x8000 cp linux/arch/arm/boot/zImage build/zImage
Function | File |
---|---|
PlutoSDR Rev.A Device Tree | zynq-pluto-sdr.dts |
PlutoSDR Rev.B Device Tree | zynq-pluto-sdr-revb.dts |
make -C linux -j 8 ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- zynq-pluto-sdr.dtb cp linux/arch/arm/boot/dts/zynq-pluto-sdr.dtb build/zynq-pluto-sdr.dtb make -C linux -j 8 ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- zynq-pluto-sdr-revb.dtb cp linux/arch/arm/boot/dts/zynq-pluto-sdr-revb.dtb build/zynq-pluto-sdr-revb.dtb
Function | File |
---|---|
PlutoSDR Buildroot Config | zynq_pluto_defconfig |
make -C buildroot ARCH=arm zynq_pluto_defconfig make -C buildroot TOOLCHAIN_EXTERNAL_INSTALL_DIR= ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- BUSYBOX_CONFIG_FILE=/home/michael/devel/pluto/plutosdr-fw/buildroot/board/pluto/busybox-1.25.0.config all cp buildroot/output/images/rootfs.cpio.gz build/rootfs.cpio.gz
Function | File |
---|---|
Pluto HDL Project | Files |
source /opt/Xilinx/Vivado/2016.2/settings64.sh make -C hdl/projects/pluto cp hdl/projects/pluto/pluto.sdk/system_top.hdf build/system_top.hdf
Function | File |
---|---|
Create FSBL TCL script | create_fsbl_project.tcl |
source /opt/Xilinx/Vivado/2016.2/settings64.sh xsdk -batch -source scripts/create_fsbl_project.tcl cp build/sdk/hw_0/system_top.bit build/system_top.bit
Function | File |
---|---|
PlutoSDR Image Tree Source | pluto.its |
u-boot-xlnx/tools/mkimage -f scripts/pluto.its build/pluto.itb
cp build/pluto.itb build/pluto.itb.tmp dfu-suffix -a build/pluto.itb.tmp -v 0x0456 -p 0xb673 mv build/pluto.itb.tmp build/pluto.dfu
md5sum build/pluto.itb | cut -d ' ' -f 1 > build/pluto.frm.md5 cat build/pluto.itb build/pluto.frm.md5 > build/pluto.frm
Function | File |
---|---|
PlutoSDR u-boot Config | zynq_pluto_defconfig |
PlutoSDR u-boot Device Tree | zynq-pluto-sdr.dts |
make -C u-boot-xlnx ARCH=arm zynq_pluto_defconfig make -C u-boot-xlnx ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- UBOOTVERSION="PlutoSDR v0.20-PlutoSDR" cp u-boot-xlnx/u-boot build/u-boot.elf
echo img:{[bootloader] build/sdk/fsbl/Release/fsbl.elf build/u-boot.elf } > build/boot.bif source /opt/Xilinx/Vivado/2016.2/settings64.sh bootgen -image build/boot.bif -w -o build/boot.bin
cp build/boot.bin build/boot.bin.tmp dfu-suffix -a build/boot.bin.tmp -v 0x0456 -p 0xb673 mv build/boot.bin.tmp build/boot.dfu
CROSS_COMPILE=arm-xilinx-linux-gnueabi- scripts/get_default_envs.sh > build/uboot-env.txt u-boot-xlnx/tools/mkenvimage -s 0x20000 -o build/uboot-env.bin build/uboot-env.txt
cp build/uboot-env.bin build/uboot-env.bin.tmp dfu-suffix -a build/uboot-env.bin.tmp -v 0x0456 -p 0xb673 mv build/uboot-env.bin.tmp build/uboot-env.dfu
cat build/boot.bin build/uboot-env.bin scripts/target_mtd_info.key | tee build/boot.frm | md5sum | cut -d ' ' -f1 | tee -a build/boot.frm