This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:tools:m2k [15 Aug 2019 14:05] – remove source measure unit to describe m2k Doug Mercer | university:tools:m2k [16 Aug 2019 00:58] – Deleted extra space so that ordered list reads 1, 2 rather than 1,1 Matt Duff | ||
---|---|---|---|
Line 22: | Line 22: | ||
* ADALM2000 users normally interact with real world analog signals using [[university: | * ADALM2000 users normally interact with real world analog signals using [[university: | ||
* Everyone should read this section, as it describes the device, and describes how to get the drivers and host software installed properly. | * Everyone should read this section, as it describes the device, and describes how to get the drivers and host software installed properly. | ||
- | |||
- [[./ | - [[./ | ||
* normally write custom software or HDL (for the FPGA) that run directly on the ADALM2000 device. This may put the ADALM2000 in different modes, and support different external USB devices (including LAN (via USB), or WiFi (vs USB)), extending the capabilities of the device. This includes all the information to compile HDL projects, compile kernels, change to custom USB PID/VID and/or run custom user space applications. | * normally write custom software or HDL (for the FPGA) that run directly on the ADALM2000 device. This may put the ADALM2000 in different modes, and support different external USB devices (including LAN (via USB), or WiFi (vs USB)), extending the capabilities of the device. This includes all the information to compile HDL projects, compile kernels, change to custom USB PID/VID and/or run custom user space applications. |