This is an old revision of the document!
In order to be able to process radio signals with ADALM2000 is necessary a receiver that can convert the incoming RF signal to a lower intermediate frequency. The FM signal, centered on a carrier frequency with high values, is reduced to an intermediate value, called IF, through a downconverter receiver. The receiver built for the m2k-radio has a basic radio architecture with four main components: Antenna, Low noise amplifier, Mixer and a Local oscillator. These 3 main parts need additional components (usually some filters) in order to work well together and receive signals in certain desired bandwidths.
Figure 1. Block Schematic of the M2k Receiver
For building a first prototype, it is possible to find each block in the form of an EVAL-board which has all the necessary components already integrated and is ready to be easily used in the project. The blocks are interconnected with SMA connectors. The filters between the blocks can be used to reduce the unwanted frequencies so the acquired signal is at a better quality.
Figure 2. EVAL Boards
The last thing necessary, from a hardware point of view, is the power supply. Using an external supply and some voltage regulators is possible to implement an easy solution. In this case, with a 12V supply and simple voltage regulators together with their bypass capacitors you can implement the 5V and 9V supplies needed for the boards.
Figure 3. Power Supplies schematic
Figure 4. Power Supplies breadboard connections
The outputs of the regulators should be connected on the corresponding VCC pins/pads of each board (5V for LNA and PLL, 9V for the mixer).
1+ - AD831 IFout 1- - AD831 GND (outer part of the SMA connector) 2+ - 2- - W1 – DIO0 - ADF4351 CLK DIO1 - ADF4351 DATA DIO2 - ADF4351 LE DIO3 - ADF4351 MUXOUT
Figure 5. M2k Pinout
Figure 6. M2k Radio Receiver
GNU Radio is a free and open-source software development toolkit that provides signal processing blocks to implement software radios. GNU Radio Companion (GRC) is a graphical tool for creating signal flow graphs and generating flow-graph source code. GNU Radio can be extended with own functionality and blocks using OutOfTreeModules. gr-iio is a module containing IIO blocks for GNU Radio.
Creating a flowgraph in GRC, using GNU Radio 3.7, is an easy and fast solution. There are two possible approaches:
All steps for integrating ADF4350 with gr-iio will be further explained.
Controlling the radio implies controlling the output voltage frequency of ADF4350. A GRC block, integrated with IIO blocks, that controls the frequency can be created. no-OS provides a driver for ADF4350 that simplifies the work. This driver communicates using SPI. In the following steps we are going to create a GRC block for gr-iio that uses libm2k communication segment integrated with no-OS drivers.
The steps to implement a GRC block:
Project structure:
Create the inclusion header
Create adf4350_sink.h in gr-iio/include/gnuradio/iio.
Add this file in the corresponding CMake file.
install(FILES ... adf4350_sink.h DESTINATION ${GR_INCLUDE_DIR}/gnuradio/iio)
In the make function add as parameters the URI and all attributes from the adf4350_init_param structure (23 attributes) found in the driver. This way they could be change from GRC without hard coding them.
Create the implementation class
In this part we are going to integrate libm2k with a no-OS driver. For more information please check this link.
Create adf4350_sink_impl.h and adf4350_sink_impl.cc in gr-iio/lib. Create a drives directory in gr-iio/lib and add the ADF4350 driver. Add both source files in the corresponding CMake file.
list(APPEND iio_sources ... adf4350_sink_impl.cc drivers/adf4350.c)
Create a header called spi.h and include the SPI header of libm2k:
//spi.h #include <libm2k/tools/spi.hpp>
ADF4350 block will receive a message from an IIO Attribute Updater block every 1 ms. The message contains the value of the frequency. The adf4350_sink_impl class has to implement the class constructor and a method (write_attribute) that will receive the message and will communicate with the chip in order to set its output frequency.
In the source file (adf4350_sink_impl.cc) include the SPI extra header of libm2k (<libm2k/tools/spi_extra.hpp>). In the constructor open the context and initialize m2k_spi_init structure :
libm2k::contexts::M2k *context = libm2k::contexts::m2kOpen(uri.c_str()); m2k_spi_init m2KSpiInit; m2KSpiInit.clock = 0; m2KSpiInit.mosi = 1; m2KSpiInit.miso = 7; m2KSpiInit.bit_numbering = MSB; m2KSpiInit.context = context;
Initialize the adf4350 structure with the given parameters. The first parameter, spi_init_param, should contain these values:
{ 1000000, 2, SPI_MODE_0, (void*)&m2KSpiInit }
write_attribute function is supposed to:
long long freq; pmt::pmt_t keys; if (!is_dict(pdu)) throw std::runtime_error("Message not a dictionary!\n"); keys = pmt::dict_keys(pdu); freq = std::stoll(pmt::symbol_to_string(pmt::dict_ref(pdu, pmt::nth(0, keys), pmt::PMT_NIL))); adf4350_out_altvoltage0_frequency(adf4350_device, freq);
Create python bindings
In swig directory is a file called iio_swig.i. Include the block's header in this file:
%{ ... #include "gnuradio/iio/adf4350_sink.h" %} ... %include "gnuradio/iio/adf4350_sink.h" ... GR_SWIG_BLOCK_MAGIC2(iio, adf4350_sink);
Create the GRC component
GNU Radio 3.7 uses xml files for creating GRC blocks. Create a file iio_adf4350_sink.xml in the grc directory. This file will describe how the GRC block should look like. Add all parameters using the following format:
<param> <name>name</name> <key>key</key> <value>val</value> <type>type</type> <hide>part</hide> <!-- optional --> </param>
This block is a sink for messages, not streams. To specify this create the following tag:
<sink> <name>attr</name> <type>message</type> <optional>1</optional> </sink>
Build the new created block
cmake . make sudo make install cd .. sudo ldconfig
The source code can be found on the gr-iio github page, grcon2019_m2k branch.