This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:tools:m2k:tutorials:buildingaradiowithm2k [26 Feb 2020 12:34] – replace gr-iio with gr-m2k Teo Perisanu | university:tools:m2k:tutorials:buildingaradiowithm2k [26 Feb 2020 14:04] – change zip Teo Perisanu | ||
---|---|---|---|
Line 202: | Line 202: | ||
{{: | {{: | ||
- | The file {{ : | + | The file {{ : |
The gnuradio flowgraph acquires the data from the M2K and sets the ADF4350 PLL frequency. When changing the PLL frequency slider, the gnuradio ADF4350 block that we just written, encodes SPI messages to the PLL in order to change the frequency that is fed into the mixer. | The gnuradio flowgraph acquires the data from the M2K and sets the ADF4350 PLL frequency. When changing the PLL frequency slider, the gnuradio ADF4350 block that we just written, encodes SPI messages to the PLL in order to change the frequency that is fed into the mixer. | ||
The data acquired from the mixer is captured by the M2k using GNURadio. The flow then shifts the frequency by a smaller offset in the " | The data acquired from the mixer is captured by the M2k using GNURadio. The flow then shifts the frequency by a smaller offset in the " | ||
This project was presented in GRCon 2019. Slides are available [[https:// | This project was presented in GRCon 2019. Slides are available [[https:// |