This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:m2k:scopy [11 Jun 2018 12:35] – add Scripting Guide Antoniu Miclaus | university:tools:m2k:scopy [28 Sep 2022 22:11] (current) – [Download] Adrian Suciu | ||
---|---|---|---|
Line 2: | Line 2: | ||
===== About ===== | ===== About ===== | ||
- | Scopy is a multi-functional software toolset with strong capabilities for signal analysis. | + | Scopy is a multi-functional software toolset with strong capabilities for signal analysis. |
===== Download ===== | ===== Download ===== | ||
<WRAP round download> | <WRAP round download> | ||
**Scopy for Windows ** | **Scopy for Windows ** | ||
- | * Download: [[https:// | + | * Download: [[https:// |
- | * Download: [[https:// | + | |
**Scopy for Linux ** | **Scopy for Linux ** | ||
Line 15: | Line 14: | ||
**Scopy for OSX ** | **Scopy for OSX ** | ||
* Download: [[https:// | * Download: [[https:// | ||
+ | |||
+ | **Scopy for Android ** | ||
+ | * Download: [[https:// | ||
+ | * Google Play store link: [[https:// | ||
+ | |||
+ | **Scopy all platforms latest(nightly) builds ** | ||
+ | * Download: [[https:// | ||
+ | |||
</ | </ | ||
- | <WRAP round important> | + | <WRAP round important> |
- | * [[university: | + | * [[university: |
</ | </ | ||
Line 25: | Line 32: | ||
=== Scopy for Windows === | === Scopy for Windows === | ||
Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | ||
+ | === Video === | ||
+ | {{youtube> | ||
\\ | \\ | ||
=== Scopy for Linux === | === Scopy for Linux === | ||
- | Before downloading and extracting the scopy_v1.0-linux.zip archive, you need to setup Flatpak using [[https:// | + | Before downloading and extracting the scopy-v1.1.1-Linux-flatpak.zip archive, you need to setup Flatpak using [[https:// |
For Ubuntu, you can use the following steps: | For Ubuntu, you can use the following steps: | ||
Line 41: | Line 49: | ||
< | < | ||
- | **flatpak install | + | **flatpak install |
</ | </ | ||
+ | === Video === | ||
+ | {{youtube> | ||
\\ | \\ | ||
=== Scopy for OSX === | === Scopy for OSX === | ||
Double click the downloaded .dmg to make its content available. " | Double click the downloaded .dmg to make its content available. " | ||
Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\ | Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\ | ||
+ | |||
+ | === Video === | ||
+ | {{youtube> | ||
+ | \\ | ||
+ | === Scopy for Android === | ||
+ | Tap on the downloaded .apk file to start the installation process and proceed by hitting the " | ||
+ | In order to connect [[adi> | ||
+ | \\ | ||
+ | <WRAP centeralign> | ||
+ | \\ | ||
===== Launching ===== | ===== Launching ===== | ||
Line 122: | Line 142: | ||
The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window. | The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window. | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
</ | </ | ||
+ | |||
+ | === Detaching Instruments === | ||
+ | |||
+ | Scopy provides the detaching into multiple windows feature for each instrument available, providing a better view/ | ||
+ | |||
+ | There are 2 ways to do this: | ||
+ | - __Drag and Drop__ - select the desired instrument drag it outside Instrument Menu section and drop it inside the application window area. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | </ | ||
+ | |||
+ | - __Double Click__ - first make sure that the **Double click to detach a tool** option is enabled in the **Preferences** menu; double-click on the desired instrument to detach it. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | </ | ||
+ | |||
\\ | \\ | ||
- | ==== Instruments ==== | + | ==== Instruments |
+ | |||
+ | <WRAP centeralign> | ||
+ | </ | ||
Complete user guides on how to use each Scopy instrument: | Complete user guides on how to use each Scopy instrument: |