university:tools:m2k:scopy [16 May 2018 16:41]
Alexandra Trifan Add link to osx build guide
university:tools:m2k:scopy [08 Feb 2021 14:50] (current)
Alexandra Trifan Update link to ADALM2000 for End users page
Line 2: Line 2:
  
 ===== About ===== ===== About =====
-Scopy is a multi-functional software toolset with strong capabilities for signal analysis.+Scopy is a multi-functional software toolset with strong capabilities for signal analysis. ​If you are interested in some [[./​scopy/​screen shots]]
 ===== Download ===== ===== Download =====
 <WRAP round download>​ <WRAP round download>​
-  * **Scopy for Windows ​- Alpha Release** + 
-  * Download: [[https://​github.com/​analogdevicesinc/​scopy/​releases/​latest| Windows ​32/64-bit ​installer]] +**Scopy for Windows ** 
-  * Download: [[https://ci.appveyor.com/api/projects/​analogdevicesinc/​scopy/​artifacts/scopy-setup.exe?​branch=master| Installer for latest (nightly) build (Windows 32/64-bit)]]+  * Download: [[https://​github.com/​analogdevicesinc/​scopy/​releases/​latest| ​Installer for latest release (Windows 64/32-bit)]] 
 + 
 +**Scopy for Linux ** 
 +  * Download: [[https://github.com/analogdevicesinc/scopy/​releases/​latest| Scopy Flatpak installer]] 
 + 
 +**Scopy for OSX ** 
 +  * Download: [[https://​github.com/​analogdevicesinc/​scopy/​releases/latest| OSX installer]] 
 + 
 +**Scopy all platforms latest(nightly) builds ** 
 +  * Download: [[https://​ci.appveyor.com/​project/​analogdevicesinc/​scopy| Installer for latest (nightly) build]] 
 </​WRAP>​ </​WRAP>​
  
-<WRAP round important>​In order to have Scopy working with [[http://​www.analog.com/​en/​design-center/​evaluation-hardware-and-software/​evaluation-boards-kits/​ADALM2000.html|ADALM2000]] please make sure that the Device Drivers are installed. A guide on this topic can be found in the section: +<WRAP round important>​In order to have Scopy working with [[adi>ADALM2000]] please make sure that the Device Drivers are installed. A guide on this topic can be found in the section: 
-  * [[university:​tools:​adalm2000:users|ADALM-2000 ​for End Users]].+  * [[university:​tools:​m2k:users|ADALM2000 ​for End Users]].
 </​WRAP>​ </​WRAP>​
  
 ===== Installation ===== ===== Installation =====
 +
 +=== Scopy for Windows ===
 Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required.
 +=== Video === 
 +{{youtube>​894HkVXf7-U}}
 +\\
 +=== Scopy for Linux ===
 +Before downloading and extracting the scopy-v1.1.1-Linux-flatpak.zip archive, you need to setup Flatpak using [[https://​flatpak.org/​setup/​ | this setup guide]] for your Linux distribution.
 +
 +For Ubuntu, you can use the following steps:
 +<​xterm>​
 +    **sudo add-apt-repository ppa:​alexlarsson/​flatpak
 +    sudo apt update
 +    sudo apt install flatpak
 +    flatpak remote-add --if-not-exists flathub https://​flathub.org/​repo/​flathub.flatpakrepo**
 +</​xterm>​
 +
 +After this, get the **Scopy.flatpak** file from the downloaded archive and run:
 +
 +<​xterm>​
 +    **flatpak install scopy-v1.1.1-Linux-flatpak.flatpak**
 +</​xterm>​
 +
 +=== Video === 
 +{{youtube>​9qgxmmTrcSE}}
 +\\
 +=== Scopy for OSX ===
 +Double click the downloaded .dmg to make its content available. "​Scopy"​ will show up in the Finder sidebar and a window showing the content should open up. \\
 +Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\
 +
 +=== Video === 
 +{{youtube>​To0ACQ77tkg}}
 +
 ===== Launching ===== ===== Launching =====
-Run Scopy from the Desktop Shortcut / Start Menu / Installation Folder ​(Scopy.exe).\\+Run Scopy from the Desktop Shortcut / Start Menu / Installation Folder. \\ 
 + 
 +On Linux, you can also run it using: 
 +<​xterm>​ 
 +    **flatpak run org.adi.Scopy** 
 +</​xterm>​
  
 ====== Using the Application ===== ====== Using the Application =====
Line 77: Line 124:
  
 \\ \\
-===== Instruments ​=====+===== User Guides ​=====
  
 Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application,​ a list of instruments that are available for that device will be enabled. Each instrument can be opened from the left menu. Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application,​ a list of instruments that are available for that device will be enabled. Each instrument can be opened from the left menu.
Line 84: Line 131:
 The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window. The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window.
  
-<WRAP centeralign>​{{:​university:​tools:​m2k:​scopy_instruments_menu.png| Scopy Home View}}+<WRAP centeralign>​{{:​university:​tools:​m2k:​min_menu.png| Scopy Minimized Menu View}}
 </​WRAP>​ </​WRAP>​
  
-==== Instruments ​User Guides ​====+=== Detaching Instruments === 
 + 
 +Scopy provides the detaching into multiple windows feature for each instrument available, providing a better view/​manipulation. 
 + 
 +There are 2 ways to do this: 
 +  - __Drag and Drop__ - select the desired instrument drag it outside Instrument Menu section and drop it inside the application window area. 
 + 
 +<WRAP centeralign>​{{:​university:​tools:​m2k:​scopy_drag_n_drop.gif| Scopy Drag and Drop}} 
 +</​WRAP>​ 
 + 
 +  - __Double Click__ - first make sure that the **Double click to detach a tool** option is enabled in the **Preferences** menu; double-click on the desired instrument to detach it.  
 + 
 +<WRAP centeralign>​{{:​university:​tools:​m2k:​scopy_dc_detach.gif| Scopy Double Click Detach}} 
 +</​WRAP>​ 
 + 
 +\\ 
 +==== Instruments ​Overview==== 
 + 
 +<WRAP centeralign>​{{:​university:​tools:​m2k:​scopy_instruments_menu.png| Scopy Home View}} 
 +</​WRAP>​
  
 Complete user guides on how to use each Scopy instrument: Complete user guides on how to use each Scopy instrument:
Line 100: Line 166:
   - [[university:​tools:​m2k:​scopy:​power-supply|Power Supply]]   - [[university:​tools:​m2k:​scopy:​power-supply|Power Supply]]
  
 +==== Scripts ====
 +
 +User guide on how to use scripts with Scopy:
 +  * [[university:​tools:​m2k:​scopy:​scripting-guide|Scopy - Scripting Guide]]
 \\ \\
 ====== Building ====== ====== Building ======
university/tools/m2k/scopy.1526481679.txt.gz · Last modified: 16 May 2018 16:41 by Alexandra Trifan