This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:m2k:scopy [10 May 2018 17:22] – minor edit + new Scopy shots Antoniu Miclaus | university:tools:m2k:scopy [30 May 2018 15:52] – Adrian Suciu | ||
---|---|---|---|
Line 5: | Line 5: | ||
===== Download ===== | ===== Download ===== | ||
<WRAP round download> | <WRAP round download> | ||
- | * **Scopy for Windows | + | |
+ | **Scopy for Windows ** | ||
* Download: [[https:// | * Download: [[https:// | ||
* Download: [[https:// | * Download: [[https:// | ||
+ | |||
+ | **Scopy for Linux ** | ||
+ | * Download: [[https:// | ||
+ | |||
+ | **Scopy for OSX ** | ||
+ | * Download: [[https:// | ||
</ | </ | ||
Line 15: | Line 22: | ||
===== Installation ===== | ===== Installation ===== | ||
+ | |||
+ | === Scopy for Windows === | ||
Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | ||
+ | |||
+ | \\ | ||
+ | === Scopy for Linux === | ||
+ | Before downloading and extracting the scopy_v1.0-linux.zip archive, you need to setup Flatpak using [[https:// | ||
+ | |||
+ | For Ubuntu, you can use the following steps: | ||
+ | < | ||
+ | **sudo add-apt-repository ppa: | ||
+ | sudo apt update | ||
+ | sudo apt install flatpak | ||
+ | flatpak remote-add --if-not-exists flathub https:// | ||
+ | </ | ||
+ | |||
+ | After this, get the **Scopy.flatpak** file from the downloaded archive and run: | ||
+ | |||
+ | < | ||
+ | **flatpak install Scopy.flatpak** | ||
+ | </ | ||
+ | |||
+ | \\ | ||
+ | === Scopy for OSX === | ||
+ | Double click the downloaded .dmg to make its content available. " | ||
+ | Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\ | ||
+ | |||
===== Launching ===== | ===== Launching ===== | ||
- | Run Scopy from the Desktop Shortcut / Start Menu / Installation Folder | + | Run Scopy from the Desktop Shortcut / Start Menu / Installation Folder. \\ |
+ | |||
+ | On Linux, you can also run it using: | ||
+ | < | ||
+ | **flatpak run org.adi.Scopy** | ||
+ | </ | ||
====== Using the Application ===== | ====== Using the Application ===== | ||
Line 106: | Line 144: | ||
- [[university: | - [[university: | ||
- [[university: | - [[university: | ||
+ | - [[university: | ||