Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
university:tools:m2k:scopy [04 Feb 2021 11:06] – Change nightly build link Adrian Suciuuniversity:tools:m2k:scopy [28 Sep 2022 22:11] (current) – [Download] Adrian Suciu
Line 8: Line 8:
 **Scopy for Windows ** **Scopy for Windows **
   * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| Installer for latest release (Windows 64/32-bit)]]   * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| Installer for latest release (Windows 64/32-bit)]]
-  * Download: [[https://ci.appveyor.com/project/analogdevicesinc/scopy| Installer for latest (nightly) build] 
  
 **Scopy for Linux ** **Scopy for Linux **
Line 15: Line 14:
 **Scopy for OSX ** **Scopy for OSX **
   * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| OSX installer]]   * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| OSX installer]]
 +
 +**Scopy for Android **
 +  * Download: [[https://github.com/analogdevicesinc/scopy/releases/latest| Android installer]]
 +  * Google Play store link: [[https://play.google.com/store/apps/details?id=org.adi.scopy|Scopy]]
 +
 +**Scopy all platforms latest(nightly) builds **
 +  * Download: [[https://github.com/analogdevicesinc/scopy/releases/tag/continous| Installer for latest (nightly) build]]
 +
 </WRAP> </WRAP>
  
 <WRAP round important>In order to have Scopy working with [[adi>ADALM2000]] please make sure that the Device Drivers are installed. A guide on this topic can be found in the section: <WRAP round important>In order to have Scopy working with [[adi>ADALM2000]] please make sure that the Device Drivers are installed. A guide on this topic can be found in the section:
-  * [[university:tools:adalm2000:users|ADALM2000 for End Users]].+  * [[university:tools:m2k:users|ADALM2000 for End Users]].
 </WRAP> </WRAP>
  
Line 54: Line 61:
 === Video ===  === Video === 
 {{youtube>To0ACQ77tkg}} {{youtube>To0ACQ77tkg}}
 +\\
 +=== Scopy for Android ===
 +Tap on the downloaded .apk file to start the installation process and proceed by hitting the "Install" button. Optionally, you may be warned that this application comes from unknown sources, hit the "Install anyway" button. Now, you can find "Scopy" together with your other apps. \\
 +In order to connect [[adi>ADALM2000]] to your device, you will need an OTG adapter that will mediate the connection between your device and the USB cable, as shown in the image below.
 +\\
 +<WRAP centeralign>{{:university:tools:m2k:scopy-android-setup-example.png | Scopy Android setup }}</WRAP>
 +\\ 
  
 ===== Launching ===== ===== Launching =====
university/tools/m2k/scopy.txt · Last modified: 28 Sep 2022 22:11 by Adrian Suciu