This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:m2k:scopy [13 Feb 2019 11:05] – add detach instrument section Antoniu Miclaus | university:tools:m2k:scopy [31 Jul 2019 16:19] – Update installer links Guramulta Daniel | ||
---|---|---|---|
Line 7: | Line 7: | ||
**Scopy for Windows ** | **Scopy for Windows ** | ||
- | * Download: [[https:// | + | * Download: [[https:// |
- | * Download: [[https://ci.appveyor.com/api/ | + | * Download: [[https://tinyurl.com/yyfa4ytt| Installer for latest (nightly) build (Windows 64-bit)]] |
+ | * Download: [[https://tinyurl.com/ | ||
**Scopy for Linux ** | **Scopy for Linux ** | ||
Line 127: | Line 128: | ||
=== Detaching Instruments === | === Detaching Instruments === | ||
- | Scopy provides the detaching into multiple windows feature for each Instrument availabl, providing a better view/ | + | Scopy provides the detaching into multiple windows feature for each instrument available, providing a better view/ |
There are 2 ways to do this: | There are 2 ways to do this: | ||
Line 135: | Line 136: | ||
</ | </ | ||
- | - __Double Click__ - first, make sure that the **Double click to detach a tool** option is enabled in the **Preferences** menu; double-click on the desired instrument to detach it. | + | - __Double Click__ - first make sure that the **Double click to detach a tool** option is enabled in the **Preferences** menu; double-click on the desired instrument to detach it. |
- | <WRAP centeralign> | + | <WRAP centeralign> |
</ | </ | ||