This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:m2k:scopy [30 May 2018 15:52] – Adrian Suciu | university:tools:m2k:scopy [13 Feb 2019 11:05] – add detach instrument section Antoniu Miclaus | ||
---|---|---|---|
Line 18: | Line 18: | ||
<WRAP round important> | <WRAP round important> | ||
- | * [[university: | + | * [[university: |
</ | </ | ||
Line 115: | Line 115: | ||
\\ | \\ | ||
- | ===== Instruments | + | ===== User Guides |
Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, | Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, | ||
Line 122: | Line 122: | ||
The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window. | The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window. | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
</ | </ | ||
- | ==== Instruments | + | === Detaching Instruments === |
+ | |||
+ | Scopy provides the detaching into multiple windows feature for each Instrument availabl, providing a better view/ | ||
+ | |||
+ | There are 2 ways to do this: | ||
+ | - __Drag and Drop__ - select the desired instrument drag it outside Instrument Menu section and drop it inside the application window area. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | </ | ||
+ | |||
+ | - __Double Click__ - first, make sure that the **Double click to detach a tool** option is enabled in the **Preferences** menu; double-click on the desired instrument to detach it. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | </ | ||
+ | |||
+ | \\ | ||
+ | ==== Instruments | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | </ | ||
Complete user guides on how to use each Scopy instrument: | Complete user guides on how to use each Scopy instrument: | ||
Line 138: | Line 157: | ||
- [[university: | - [[university: | ||
+ | ==== Scripts ==== | ||
+ | |||
+ | User guide on how to use scripts with Scopy: | ||
+ | * [[university: | ||
\\ | \\ | ||
====== Building ====== | ====== Building ====== |