This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:m2k:scopy [16 May 2018 16:41] – Add link to osx build guide Alexandra Trifan | university:tools:m2k:scopy [22 Mar 2022 14:26] – Added Android instructions and fixed link to nightly builds Ioana Chelaru | ||
---|---|---|---|
Line 2: | Line 2: | ||
===== About ===== | ===== About ===== | ||
- | Scopy is a multi-functional software toolset with strong capabilities for signal analysis. | + | Scopy is a multi-functional software toolset with strong capabilities for signal analysis. |
===== Download ===== | ===== Download ===== | ||
<WRAP round download> | <WRAP round download> | ||
- | * **Scopy for Windows | + | |
- | * Download: [[https:// | + | **Scopy for Windows ** |
- | * Download: [[https://ci.appveyor.com/api/projects/ | + | * Download: [[https:// |
+ | |||
+ | **Scopy for Linux ** | ||
+ | * Download: [[https://github.com/analogdevicesinc/scopy/ | ||
+ | |||
+ | **Scopy for OSX ** | ||
+ | * Download: [[https:// | ||
+ | |||
+ | **Scopy for Android ** | ||
+ | * Download: [[https:// | ||
+ | |||
+ | **Scopy all platforms latest(nightly) builds ** | ||
+ | * Download: [[https:// | ||
</ | </ | ||
- | <WRAP round important> | + | <WRAP round important> |
- | * [[university: | + | * [[university: |
</ | </ | ||
===== Installation ===== | ===== Installation ===== | ||
+ | |||
+ | === Scopy for Windows === | ||
Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | ||
+ | === Video === | ||
+ | {{youtube> | ||
+ | \\ | ||
+ | === Scopy for Linux === | ||
+ | Before downloading and extracting the scopy-v1.1.1-Linux-flatpak.zip archive, you need to setup Flatpak using [[https:// | ||
+ | |||
+ | For Ubuntu, you can use the following steps: | ||
+ | < | ||
+ | **sudo add-apt-repository ppa: | ||
+ | sudo apt update | ||
+ | sudo apt install flatpak | ||
+ | flatpak remote-add --if-not-exists flathub https:// | ||
+ | </ | ||
+ | |||
+ | After this, get the **Scopy.flatpak** file from the downloaded archive and run: | ||
+ | |||
+ | < | ||
+ | **flatpak install scopy-v1.1.1-Linux-flatpak.flatpak** | ||
+ | </ | ||
+ | |||
+ | === Video === | ||
+ | {{youtube> | ||
+ | \\ | ||
+ | === Scopy for OSX === | ||
+ | Double click the downloaded .dmg to make its content available. " | ||
+ | Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\ | ||
+ | |||
+ | === Video === | ||
+ | {{youtube> | ||
+ | \\ | ||
+ | === Scopy for Android === | ||
+ | Tap on the downloaded .apk file to start the installation process and proceed by hitting the " | ||
+ | In order to connect Adalm2000 to your device, you will need an OTG adaptor that will mediate the connection between your device and the USB cable. | ||
+ | \\ | ||
+ | |||
===== Launching ===== | ===== Launching ===== | ||
- | Run Scopy from the Desktop Shortcut / Start Menu / Installation Folder | + | Run Scopy from the Desktop Shortcut / Start Menu / Installation Folder. \\ |
+ | |||
+ | On Linux, you can also run it using: | ||
+ | < | ||
+ | **flatpak run org.adi.Scopy** | ||
+ | </ | ||
====== Using the Application ===== | ====== Using the Application ===== | ||
Line 77: | Line 132: | ||
\\ | \\ | ||
- | ===== Instruments | + | ===== User Guides |
Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, | Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, | ||
Line 84: | Line 139: | ||
The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window. | The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window. | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
</ | </ | ||
- | ==== Instruments | + | === Detaching Instruments === |
+ | |||
+ | Scopy provides the detaching into multiple windows feature for each instrument available, providing a better view/ | ||
+ | |||
+ | There are 2 ways to do this: | ||
+ | - __Drag and Drop__ - select the desired instrument drag it outside Instrument Menu section and drop it inside the application window area. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | </ | ||
+ | |||
+ | - __Double Click__ - first make sure that the **Double click to detach a tool** option is enabled in the **Preferences** menu; double-click on the desired instrument to detach it. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | </ | ||
+ | |||
+ | \\ | ||
+ | ==== Instruments | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | </ | ||
Complete user guides on how to use each Scopy instrument: | Complete user guides on how to use each Scopy instrument: | ||
Line 100: | Line 174: | ||
- [[university: | - [[university: | ||
+ | ==== Scripts ==== | ||
+ | |||
+ | User guide on how to use scripts with Scopy: | ||
+ | * [[university: | ||
\\ | \\ | ||
====== Building ====== | ====== Building ====== |