This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:m2k:scopy [16 May 2018 16:41] – Add link to osx build guide Alexandra Trifan | university:tools:m2k:scopy [11 Jun 2018 12:35] – add Scripting Guide Antoniu Miclaus | ||
---|---|---|---|
Line 5: | Line 5: | ||
===== Download ===== | ===== Download ===== | ||
<WRAP round download> | <WRAP round download> | ||
- | * **Scopy for Windows | + | |
+ | **Scopy for Windows ** | ||
* Download: [[https:// | * Download: [[https:// | ||
* Download: [[https:// | * Download: [[https:// | ||
+ | |||
+ | **Scopy for Linux ** | ||
+ | * Download: [[https:// | ||
+ | |||
+ | **Scopy for OSX ** | ||
+ | * Download: [[https:// | ||
</ | </ | ||
Line 15: | Line 22: | ||
===== Installation ===== | ===== Installation ===== | ||
+ | |||
+ | === Scopy for Windows === | ||
Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | ||
+ | |||
+ | \\ | ||
+ | === Scopy for Linux === | ||
+ | Before downloading and extracting the scopy_v1.0-linux.zip archive, you need to setup Flatpak using [[https:// | ||
+ | |||
+ | For Ubuntu, you can use the following steps: | ||
+ | < | ||
+ | **sudo add-apt-repository ppa: | ||
+ | sudo apt update | ||
+ | sudo apt install flatpak | ||
+ | flatpak remote-add --if-not-exists flathub https:// | ||
+ | </ | ||
+ | |||
+ | After this, get the **Scopy.flatpak** file from the downloaded archive and run: | ||
+ | |||
+ | < | ||
+ | **flatpak install Scopy.flatpak** | ||
+ | </ | ||
+ | |||
+ | \\ | ||
+ | === Scopy for OSX === | ||
+ | Double click the downloaded .dmg to make its content available. " | ||
+ | Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\ | ||
+ | |||
===== Launching ===== | ===== Launching ===== | ||
- | Run Scopy from the Desktop Shortcut / Start Menu / Installation Folder | + | Run Scopy from the Desktop Shortcut / Start Menu / Installation Folder. \\ |
+ | |||
+ | On Linux, you can also run it using: | ||
+ | < | ||
+ | **flatpak run org.adi.Scopy** | ||
+ | </ | ||
====== Using the Application ===== | ====== Using the Application ===== | ||
Line 77: | Line 115: | ||
\\ | \\ | ||
- | ===== Instruments | + | ===== User Guides |
Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, | Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, | ||
Line 86: | Line 124: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
</ | </ | ||
- | + | \\ | |
- | ==== Instruments | + | ==== Instruments ==== |
Complete user guides on how to use each Scopy instrument: | Complete user guides on how to use each Scopy instrument: | ||
Line 100: | Line 138: | ||
- [[university: | - [[university: | ||
+ | ==== Scripts ==== | ||
+ | |||
+ | User guide on how to use scripts with Scopy: | ||
+ | * [[university: | ||
\\ | \\ | ||
====== Building ====== | ====== Building ====== |