Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
university:tools:m2k:scopy:voltmeter [21 May 2018 15:50] – Update screenshots Alexandra Trifanuniversity:tools:m2k:scopy:voltmeter [07 Apr 2021 22:10] (current) – adding video Brandon Bushey
Line 1: Line 1:
 ====== Scopy Voltmeter ====== ====== Scopy Voltmeter ======
 +
 +===== Video =====
 +{{youtube>kohIqwrlmjI}}
  
 ===== General Description ===== ===== General Description =====
Line 5: Line 8:
  
 Open the Voltmeter instrument by clicking on the “Voltmeter” button displayed at the far left of the Scopy window.  Open the Voltmeter instrument by clicking on the “Voltmeter” button displayed at the far left of the Scopy window. 
-The voltmeter instrument makes use of the Oscilloscope probes 1 and 2 in the M2k for the channels which are capable of measuring DC and AC signals at ±20V+The voltmeter instrument makes use of the Oscilloscope probes 1 and 2 in the M2k for the channels which are capable of measuring DC and AC signals at ±25V
  
 <WRAP round info 65%>A Calibration feature automatically starts for the Voltmeter instrument when Scopy connects to an M2k device. Manual calibration is not necessary. <WRAP round info 65%>A Calibration feature automatically starts for the Voltmeter instrument when Scopy connects to an M2k device. Manual calibration is not necessary.
Line 37: Line 40:
 \\ \\
 \\ \\
-DC Mode will display the VDC value of the signal from -20V to 20V.+DC Mode will display the VDC value of the signal from -25V to 25V.
 \\ \\
 \\ \\
university/tools/m2k/scopy/voltmeter.1526910641.txt.gz · Last modified: 21 May 2018 15:50 by Alexandra Trifan