This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:m2k:scopy:voltmeter [21 May 2018 15:50] – Update screenshots Alexandra Trifan | university:tools:m2k:scopy:voltmeter [07 Apr 2021 22:10] (current) – adding video Brandon Bushey | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Scopy Voltmeter ====== | ====== Scopy Voltmeter ====== | ||
+ | |||
+ | ===== Video ===== | ||
+ | {{youtube> | ||
===== General Description ===== | ===== General Description ===== | ||
Line 5: | Line 8: | ||
Open the Voltmeter instrument by clicking on the “Voltmeter” button displayed at the far left of the Scopy window. | Open the Voltmeter instrument by clicking on the “Voltmeter” button displayed at the far left of the Scopy window. | ||
- | The voltmeter instrument makes use of the Oscilloscope probes 1 and 2 in the M2k for the channels which are capable of measuring DC and AC signals at ±20V. | + | The voltmeter instrument makes use of the Oscilloscope probes 1 and 2 in the M2k for the channels which are capable of measuring DC and AC signals at ±25V. |
<WRAP round info 65%>A Calibration feature automatically starts for the Voltmeter instrument when Scopy connects to an M2k device. Manual calibration is not necessary. | <WRAP round info 65%>A Calibration feature automatically starts for the Voltmeter instrument when Scopy connects to an M2k device. Manual calibration is not necessary. | ||
Line 37: | Line 40: | ||
\\ | \\ | ||
\\ | \\ | ||
- | DC Mode will display the VDC value of the signal from -20V to 20V. | + | DC Mode will display the VDC value of the signal from -25V to 25V. |
\\ | \\ | ||
\\ | \\ |