Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision |
university:tools:m2k:scopy:test-cases:digitalio [26 Jul 2017 13:14] – edit voltage values for logic levels Antoniu Miclaus | university:tools:m2k:scopy:test-cases:digitalio [28 Aug 2017 14:56] – change voltmeter range Antoniu Miclaus |
---|
| ::: | 8. Monitor the voltage value via voltmeter. | {{:university:tools:m2k:scopy:test-cases:low-voltmeter.png?100|}} | On the voltmeter the voltage displayed is be between -0.050V and 0.4V. | | | ::: | 8. Monitor the voltage value via voltmeter. | {{:university:tools:m2k:scopy:test-cases:low-voltmeter.png?100|}} | On the voltmeter the voltage displayed is be between -0.050V and 0.4V. | |
| ::: | 9. Set channel 0 to logic state 1. | {{:university:tools:m2k:scopy:test-cases:high0.png?100|}} | The interface should look like in the "Step Resources" picture (left side). | | | ::: | 9. Set channel 0 to logic state 1. | {{:university:tools:m2k:scopy:test-cases:high0.png?100|}} | The interface should look like in the "Step Resources" picture (left side). | |
| ::: | 10. Monitor the voltage value via voltmeter. | {{:university:tools:m2k:scopy:test-cases:high-voltmeter.png?100|}} | On the voltmeter the voltage displayed should be between 2.9V and 3.3V. | | | ::: | 10. Monitor the voltage value via voltmeter. | {{:university:tools:m2k:scopy:test-cases:high-voltmeter.png?100|}} | On the voltmeter the voltage displayed should be between 2.9V and 3.4V. | |
| ::: | 11. Set positive power supply to voltage level between 0V and 0.8V. | {{:university:tools:m2k:scopy:test-cases:ps-low.png?100|}} | The interface should look like in the "Step Resources" picture (left side). | | | ::: | 11. Set positive power supply to voltage level between 0V and 0.8V. | {{:university:tools:m2k:scopy:test-cases:ps-low.png?100|}} | The interface should look like in the "Step Resources" picture (left side). | |
| ::: | 12. Monitor the channel 7 logic state. | {{:university:tools:m2k:scopy:test-cases:7low.png?100|}} | Channel 7 indicates logic 0 level. | | | ::: | 12. Monitor the channel 7 logic state. | {{:university:tools:m2k:scopy:test-cases:7low.png?100|}} | Channel 7 indicates logic 0 level. | |