Both sides previous revisionPrevious revisionNext revision | Previous revision |
university:tools:m2k:scopy:test-cases:digitalio [26 Jul 2017 13:14] – edit voltage values for logic levels Antoniu Miclaus | university:tools:m2k:scopy:test-cases:digitalio [12 Apr 2021 10:28] (current) – Updated pictures Julia Anjanet Pineda |
---|
^ Description ^ Test Steps ^ Steps Resources ^ Expected Results ^ | ^ Description ^ Test Steps ^ Steps Resources ^ Expected Results ^ |
| Checking individual digital pin state | 1. Set DIO 0-7 and DIO 8-15 as individual pins | {{:university:tools:m2k:scopy:test-cases:dio-individual.png?100|}} | The interface should look like in the "Step Resources" picture (left side). | | | Checking individual digital pin state | 1. Set DIO 0-7 and DIO 8-15 as individual pins | {{:university:tools:m2k:scopy:test-cases:dio-individual.png?100|}} | The interface should look like in the "Step Resources" picture (left side). | |
| ::: | 2. Set channel 0 as output | {{:university:tools:m2k:scopy:test-cases:0out.png?50|}} | The interface should look like in the "Step Resources" picture (left side). | | | ::: | 2. Set channel 0 as output | {{:university:tools:m2k:scopy:test-cases:0out.png?100|}} | The interface should look like in the "Step Resources" picture (left side). | |
| ::: | 3. Set channel 7 as input | {{:university:tools:m2k:scopy:test-cases:7in.png?50|}} | The interface should look like in the "Step Resources" picture (left side). | | | ::: | 3. Set channel 7 as input | {{:university:tools:m2k:scopy:test-cases:7in.png?100|}} | The interface should look like in the "Step Resources" picture (left side). | |
| ::: | 4. Connect digital channel 0 to channel 7 via wires. | {{:university:tools:m2k:scopy:test-cases:0-7pin_connection.png?100|}} | | | | ::: | 4. Connect digital channel 0 to channel 7 via wires. | {{:university:tools:m2k:scopy:test-cases:0-7pin_connection.png?100|}} | | |
| ::: | 5. Change the logic state of channel 0 (0/1) multiple times and monitor channel 7 state. | {{:university:tools:m2k:scopy:test-cases:high0-7.png?100|}} {{:university:tools:m2k:scopy:test-cases:low0-7.png?100|}} | When channel 0 is set to logic one, channel 7 will be automatically set to logic 1. When channel 0 is set to logic one, channel 7 will be automatically set to logic 1. | | | ::: | 5. Change the logic state of channel 0 (0/1) multiple times and monitor channel 7 state. | {{:university:tools:m2k:scopy:test-cases:high0-7.png?100|}} {{:university:tools:m2k:scopy:test-cases:low0-7.png?100|}} | When channel 0 is set to logic one, channel 7 will be automatically set to logic 1. When channel 0 is set to logic one, channel 7 will be automatically set to logic 1. | |
| ::: | 8. Monitor the voltage value via voltmeter. | {{:university:tools:m2k:scopy:test-cases:low-voltmeter.png?100|}} | On the voltmeter the voltage displayed is be between -0.050V and 0.4V. | | | ::: | 8. Monitor the voltage value via voltmeter. | {{:university:tools:m2k:scopy:test-cases:low-voltmeter.png?100|}} | On the voltmeter the voltage displayed is be between -0.050V and 0.4V. | |
| ::: | 9. Set channel 0 to logic state 1. | {{:university:tools:m2k:scopy:test-cases:high0.png?100|}} | The interface should look like in the "Step Resources" picture (left side). | | | ::: | 9. Set channel 0 to logic state 1. | {{:university:tools:m2k:scopy:test-cases:high0.png?100|}} | The interface should look like in the "Step Resources" picture (left side). | |
| ::: | 10. Monitor the voltage value via voltmeter. | {{:university:tools:m2k:scopy:test-cases:high-voltmeter.png?100|}} | On the voltmeter the voltage displayed should be between 2.9V and 3.3V. | | | ::: | 10. Monitor the voltage value via voltmeter. | {{:university:tools:m2k:scopy:test-cases:high-voltmeter.png?100|}} | On the voltmeter the voltage displayed should be between 2.9V and 3.4V. | |
| ::: | 11. Set positive power supply to voltage level between 0V and 0.8V. | {{:university:tools:m2k:scopy:test-cases:ps-low.png?100|}} | The interface should look like in the "Step Resources" picture (left side). | | | ::: | 11. Set positive power supply to voltage level between 0V and 0.8V. | {{:university:tools:m2k:scopy:test-cases:ps-low.png?100|}} | The interface should look like in the "Step Resources" picture (left side). | |
| ::: | 12. Monitor the channel 7 logic state. | {{:university:tools:m2k:scopy:test-cases:7low.png?100|}} | Channel 7 indicates logic 0 level. | | | ::: | 12. Monitor the channel 7 logic state. | {{:university:tools:m2k:scopy:test-cases:7low.png?100|}} | Channel 7 indicates logic 0 level. | |