The data logger tool is used to :
Pressing the “+” button will generate a new tool
Using the left side menu user can select from the available device channels that will be displayed on the plot. The data is plotted in time based on the starting time (shown in the top right of the plot), the starting time reflects when the tool started collecting data and will reset on user pressing “Clear”. The data that will be displayed is collected from the device on pressing “Run” button. The data collected will be removed on pressing “Clear” this will also reset the starting time. To use this option click “Plot” button on the bottom right
Using the left side menu user can select from the available devices, for the selected device channels last read value and the unit of measurement will be displayed in text format
To use this option click “Text” button on the bottom right
Using the left side menu user can select from the available devices, for the selected device channels last read value, minimum and maximum recorded values and the unit of measurement will be displayed in seven segment display format
To use this option click “7 Segment” button on the bottom right
The gear button in the top right corner of the plugin will open the settings allowing user to:
To save data to file there are two options
On importing data a special menu is added containing the channels from file. Each channel contains the data from the CSV file from it's column, no extra data will be added to those channels when tool is recording. By pressing the “x” button all imported data is removed. Importing data multiple times from same CSV file will override current imported data Importing data from different CSV files will create new menus like the one bellow for each file