This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:m2k:scopy:spectrumanalyzer [19 Oct 2017 10:21] – minor adjustments Antoniu Miclaus | university:tools:m2k:scopy:spectrumanalyzer [10 May 2018 07:57] – updated spectrum analyzer documentation Claudiu Pop | ||
---|---|---|---|
Line 8: | Line 8: | ||
==== Spectrum Analyzer Front Panel ==== | ==== Spectrum Analyzer Front Panel ==== | ||
\\ | \\ | ||
- | {{ : | + | |
+ | {{ : | ||
\\ | \\ | ||
- **Spectrum Analyzer Tab**: Clicking this tab brings out the Spectrum Analyzer instrument in front. The white box will allow the user to run/stop the Spectrum Analyzer while other instrument tab is open. | - **Spectrum Analyzer Tab**: Clicking this tab brings out the Spectrum Analyzer instrument in front. The white box will allow the user to run/stop the Spectrum Analyzer while other instrument tab is open. | ||
Line 16: | Line 17: | ||
- **Markers**: | - **Markers**: | ||
- **Run/Stop and Single Run**: Clicking the Run button will allow the spectrum analyzer to continuously capture data. Clicking the Single button will allow the spectrum analyzer the capture the data once. | - **Run/Stop and Single Run**: Clicking the Run button will allow the spectrum analyzer to continuously capture data. Clicking the Single button will allow the spectrum analyzer the capture the data once. | ||
+ | - **Instrument Settings**: Clicking the instrument settings button will show the instrument settings panel. | ||
+ | - **Last opened panel**: Clicking this button will bring out the last opened panel. | ||
\\ | \\ | ||
---- | ---- | ||
==== Channel Settings ==== | ==== Channel Settings ==== | ||
- | {{ : | + | {{ : |
\\ | \\ | ||
Line 58: | Line 61: | ||
</ | </ | ||
\\ | \\ | ||
+ | ---- | ||
+ | ==== Instrument Settings ==== | ||
+ | {{ : | ||
+ | |||
+ | \\ | ||
+ | Instrument settings contains the export data button. | ||
---- | ---- | ||
==== Sweep Setting ==== | ==== Sweep Setting ==== | ||
\\ | \\ | ||
- | {{ : | + | {{ : |
\\ | \\ | ||
Sweep menu allows the user to make changes on the Spectrum Analyzer’s signal plot window depending on the desired frequency to be analyzed. All the changes made applies to both channels. | Sweep menu allows the user to make changes on the Spectrum Analyzer’s signal plot window depending on the desired frequency to be analyzed. All the changes made applies to both channels. | ||
Line 69: | Line 78: | ||
- **Center Frequency**: | - **Center Frequency**: | ||
- **Span**: Sets the spectrum span to be analyzed from 0 Hz to 50MHz. | - **Span**: Sets the spectrum span to be analyzed from 0 Hz to 50MHz. | ||
- | - **Resolution Bandwidth**: Sets the frequency delta between two spectrum points. | + | - **Top Amplitude**: Sets the max amplitude to be analyzed. |
+ | - **Amplitude Rabge**: Sets the amplitude range to be analyzed. | ||
- **Units**: Sets the amplitude unit to _dBFS, dBu, dBV, Vpeak and Vrms_. | - **Units**: Sets the amplitude unit to _dBFS, dBu, dBV, Vpeak and Vrms_. | ||
+ | - **Resolution Bandwidth**: | ||
\\ | \\ | ||
---- | ---- | ||
==== Markers ==== | ==== Markers ==== | ||
\\ | \\ | ||
- | {{ : | + | {{ : |
\\ | \\ | ||
Markers allow the user to measure the amplitude on a specific frequency. Scopy allows the user to have multiple markers on each channel. The marker controls makes it flexible enough for quick spectrum measurement. | Markers allow the user to measure the amplitude on a specific frequency. Scopy allows the user to have multiple markers on each channel. The marker controls makes it flexible enough for quick spectrum measurement. |