This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:m2k:scopy:spectrumanalyzer [19 Oct 2017 08:49] – Added description on different averaging types Dann Kristofer Bautista | university:tools:m2k:scopy:spectrumanalyzer [10 May 2018 07:57] – updated spectrum analyzer documentation Claudiu Pop | ||
---|---|---|---|
Line 8: | Line 8: | ||
==== Spectrum Analyzer Front Panel ==== | ==== Spectrum Analyzer Front Panel ==== | ||
\\ | \\ | ||
- | {{ : | + | |
+ | {{ : | ||
\\ | \\ | ||
- **Spectrum Analyzer Tab**: Clicking this tab brings out the Spectrum Analyzer instrument in front. The white box will allow the user to run/stop the Spectrum Analyzer while other instrument tab is open. | - **Spectrum Analyzer Tab**: Clicking this tab brings out the Spectrum Analyzer instrument in front. The white box will allow the user to run/stop the Spectrum Analyzer while other instrument tab is open. | ||
Line 16: | Line 17: | ||
- **Markers**: | - **Markers**: | ||
- **Run/Stop and Single Run**: Clicking the Run button will allow the spectrum analyzer to continuously capture data. Clicking the Single button will allow the spectrum analyzer the capture the data once. | - **Run/Stop and Single Run**: Clicking the Run button will allow the spectrum analyzer to continuously capture data. Clicking the Single button will allow the spectrum analyzer the capture the data once. | ||
+ | - **Instrument Settings**: Clicking the instrument settings button will show the instrument settings panel. | ||
+ | - **Last opened panel**: Clicking this button will bring out the last opened panel. | ||
\\ | \\ | ||
---- | ---- | ||
==== Channel Settings ==== | ==== Channel Settings ==== | ||
- | {{ : | + | {{ : |
\\ | \\ | ||
Line 35: | Line 38: | ||
| Narrowband random signal (vibration data) | Hann | | | Narrowband random signal (vibration data) | Hann | | ||
|Unknown content | Hann | | |Unknown content | Hann | | ||
- | For the description of the __window function__ | + | For the description of the __Window Function__ |
< | < | ||
{{ : | {{ : | ||
- | * Hanning: The most commonly used window. It has an amplitude variation about 1.5dB for signals between bins and provides reasonable selectivity. Its filter roll off is not particularly steep. Hanning windows can limit the performance of the analyzer when looking at signals close together in frequency with very different amplitude. | + | |
- | * Flattop: The Flattop window improves on the amplitude accuracy of the Hanning window. Its between-bin amplitude variation is about 0.02 dB. However, the selectivity is a little worse. Unlike the Hanning, the Flattop window has a wide pass band and very steep rolloff on either side. Thus, signals appear wide but do not leak across the whole spectrum. | + | |
- | * Blackman-Harris: | + | |
- | * Kaiser : The Kaiser window, combines excellent selectivity and reasonable accuracy. The Kaiser window has the lowest side-lobes and the least broadening for non-bin frequencies. Because of these properties, it is the best window to use for measurements requiring a large dynamic range. | + | |
Visit [[https:// | Visit [[https:// | ||
</ | </ | ||
- | For the description of the __averaging types__ | + | For the description of the __Averaging Types__ |
< | < | ||
{{ : | {{ : | ||
Line 58: | Line 61: | ||
</ | </ | ||
\\ | \\ | ||
+ | ---- | ||
+ | ==== Instrument Settings ==== | ||
+ | {{ : | ||
+ | |||
+ | \\ | ||
+ | Instrument settings contains the export data button. | ||
---- | ---- | ||
==== Sweep Setting ==== | ==== Sweep Setting ==== | ||
\\ | \\ | ||
- | {{ : | + | {{ : |
\\ | \\ | ||
Sweep menu allows the user to make changes on the Spectrum Analyzer’s signal plot window depending on the desired frequency to be analyzed. All the changes made applies to both channels. | Sweep menu allows the user to make changes on the Spectrum Analyzer’s signal plot window depending on the desired frequency to be analyzed. All the changes made applies to both channels. | ||
Line 69: | Line 78: | ||
- **Center Frequency**: | - **Center Frequency**: | ||
- **Span**: Sets the spectrum span to be analyzed from 0 Hz to 50MHz. | - **Span**: Sets the spectrum span to be analyzed from 0 Hz to 50MHz. | ||
- | - **Resolution Bandwidth**: Sets the frequency delta between two spectrum points. | + | - **Top Amplitude**: Sets the max amplitude to be analyzed. |
+ | - **Amplitude Rabge**: Sets the amplitude range to be analyzed. | ||
- **Units**: Sets the amplitude unit to _dBFS, dBu, dBV, Vpeak and Vrms_. | - **Units**: Sets the amplitude unit to _dBFS, dBu, dBV, Vpeak and Vrms_. | ||
+ | - **Resolution Bandwidth**: | ||
\\ | \\ | ||
---- | ---- | ||
==== Markers ==== | ==== Markers ==== | ||
\\ | \\ | ||
- | {{ : | + | {{ : |
\\ | \\ | ||
Markers allow the user to measure the amplitude on a specific frequency. Scopy allows the user to have multiple markers on each channel. The marker controls makes it flexible enough for quick spectrum measurement. | Markers allow the user to measure the amplitude on a specific frequency. Scopy allows the user to have multiple markers on each channel. The marker controls makes it flexible enough for quick spectrum measurement. |