This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:m2k:scopy:siggen [16 May 2018 16:39] – [Generate waveform from math function] Adrian Suciu | university:tools:m2k:scopy:siggen [02 Jul 2021 10:52] (current) – Added noise description Adrian Suciu | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Scopy Signal Generator ====== | ====== Scopy Signal Generator ====== | ||
+ | ===== Video ===== | ||
+ | {{youtube> | ||
===== General Description ===== | ===== General Description ===== | ||
Line 39: | Line 41: | ||
CSV file format supports raw CSVs such as [[https:// | CSV file format supports raw CSVs such as [[https:// | ||
+ | |||
+ | < | ||
+ | |||
MAT file format only supports arrays of type real (no complex waveforms) | MAT file format only supports arrays of type real (no complex waveforms) | ||
Line 54: | Line 59: | ||
* Impulse | * Impulse | ||
- | + | The noise is only calculated once on the host, and simply added to the waveform buffer. This means that for cyclic waveforms the noise will be the same on each period. | |
- | + | ||
- | + | ||
===== Use cases ===== | ===== Use cases ===== | ||
Line 109: | Line 111: | ||
==== Generate waveform from math function ==== | ==== Generate waveform from math function ==== | ||
< | < | ||
- | {{ : | + | {{ : |
- | - Select Math mode and input a function | + | - Select Math mode and input a function |
+ | - Set sample rate to 75MSPS (this is the sample rate of the generated signal) | ||
+ | - Set record run length to 1ms. | ||
+ | - Run the signal | ||
- Monitor oscilloscope | - Monitor oscilloscope | ||
+ | |||
+ | < | ||
+ | </ | ||
</ | </ | ||
**Return to [[university: | **Return to [[university: |