Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
university:tools:m2k:scopy:oscilloscope [16 May 2018 15:49] – Add calibration info Alexandra Trifanuniversity:tools:m2k:scopy:oscilloscope [07 Apr 2021 22:06] (current) – added video Brandon Bushey
Line 6: Line 6:
 <WRAP round info 65%>A Calibration feature automatically starts for the Oscilloscope instrument when Scopy connects to an M2k device.</WRAP> <WRAP round info 65%>A Calibration feature automatically starts for the Oscilloscope instrument when Scopy connects to an M2k device.</WRAP>
  
-{{ :university:tools:m2k:scopy:osc-main1.png |Scopy Oscilloscope View}} +{{ :university:tools:m2k:scopy:osc-main1.png?600 |Scopy Oscilloscope View}} 
 +===== Video ===== 
 +{{youtube>zWX7VnKDYq4}}
 ===== General ===== ===== General =====
 The control panel slides in and out from the right side of the screen and can be opened by pressing the button The control panel slides in and out from the right side of the screen and can be opened by pressing the button
Line 96: Line 97:
 \\ \\
 \\ \\
 +===== Working with Mixed Signal View =====
 +
 +Using the same (+) button, described in the previous section, the Logic tab can be selected. Here there will be some information regarding how the Mixed Signal View will work and the option to enable it.
 +{{ university:tools:m2k:scopy:mixed_signal_1.png }}
 +After clicking enable a Logic widget should be added at the bottom. Clicking on the settings here will open a menu similar in usage to the Logic Analyzer. Here digital channels can be enabled / disabled, decoders can be added and so on. The samplerate of the digital and the number of samples to capture is computed from the parameters of the Oscilloscope
 +{{ university:tools:m2k:scopy:mixed_signal_2.png }}
 +\\
 +\\
 +
 **Return to [[university:tools:m2k:scopy|Scopy Main Page]]** **Return to [[university:tools:m2k:scopy|Scopy Main Page]]**
university/tools/m2k/scopy/oscilloscope.txt · Last modified: 07 Apr 2021 22:06 by Brandon Bushey