This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:m2k:scopy:networkanalyzer [11 Apr 2019 13:17] – [Network Analyzer - Low Pass Filter Example] Antoniu Miclaus | university:tools:m2k:scopy:networkanalyzer [11 Apr 2019 17:47] – [Network Analyzer - Low Pass Filter Example] Robin Getz | ||
---|---|---|---|
Line 105: | Line 105: | ||
===== Network Analyzer - Low Pass Filter Example ===== | ===== Network Analyzer - Low Pass Filter Example ===== | ||
- | In the following example we will show how to use the Network Analyzer to obtain the frequency response of a low pass filter circuit. | + | The following example we will show how to use the Network Analyzer to obtain the frequency response of a low pass filter circuit. When ever using the network analyzer, you need a stimulus/ |
Consider the circuit in the figure below: | Consider the circuit in the figure below: | ||
Line 111: | Line 111: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | Oscilloscope Positive Channel 1 (' | + | To characterize |
- | Oscilloscope Positive Channel | + | - the reference channel: |
+ | * the stimulus : Waveform Generator channel 1 (' | ||
+ | * the reference channel measurement: | ||
+ | - the response channel: | ||
+ | * the output | ||
- | The oscilloscope negative input channels are connected to ground. | + | Since everything in this example is ground referenced, the oscilloscope negative input channels are connected to ground. |
Breadboard connections for such a circuit are displayed below: | Breadboard connections for such a circuit are displayed below: | ||
Line 126: | Line 130: | ||
{{: | {{: | ||
- | The amplitude | + | The signal' |
**Return to [[university: | **Return to [[university: |