This is an old revision of the document!
Scopy DMG Installers for OSX are available for each release.
The oldest supported OSX version is 10.11.
You can also build Scopy from source, instead of using the provided installer. Before building Scopy on OSX systems, you need to make sure all the requirements are installed.
Setup Python
export PYTHONPATH=$(brew --prefix)/lib/python2.7/site-packages export PATH=$PATH:$(brew --prefix)/share/python
Get pip
curl https://bootstrap.pypa.io/get-pip.py > get-pip.py sudo python get-pip.py
Install dependencies using Homebrew
brew install brew-pip cmake gettext swig fftw bison autoconf automake libtool libzip glibmm doxygen python3 wget qt5 libusb sudo pip install --ignore-installed six brew pip mako brew pip cheetah
Get the latest release of libiio from here
Build and install Boost
cd ~ wget https://netcologne.dl.sourceforge.net/project/boost/boost/1.63.0/boost_1_63_0.tar.gz tar -xzvf boost_1_63_0.tar.gz cd boost_1_63_0 ./bootstrap.sh --with-libraries=date_time,filesystem,program_options,regex,system,test,thread ./b2 sudo ./b2 install
Build and install Markdown
cd ~ wget https://pypi.python.org/packages/1d/25/3f6d2cb31ec42ca5bd3bfbea99b63892b735d76e26f20dd2dcc34ffe4f0d/Markdown-2.6.8.tar.gz tar -xzvf Markdown-2.6.8.tar.gz cd Markdown-2.6.8 ./setup.py build sudo ./setup.py install
Build and install Cheetah
cd ~ wget https://pypi.python.org/packages/cd/b0/c2d700252fc251e91c08639ff41a8a5203b627f4e0a2ae18a6b662ab32ea/Cheetah-2.4.4.tar.gz tar -xzvf Cheetah-2.4.4.tar.gz cd Cheetah-2.4.4 ./setup.py build sudo ./setup.py install
Build and install Volk
cd ~ wget http://libvolk.org/releases/volk-1.3.tar.gz tar -xzvf volk-1.3.tar.gz cd volk-1.3 mkdir build && cd build cmake .. make sudo make install
Build and install GNU Radio
cd ~ git clone https://github.com/analogdevicesinc/gnuradio cd gnuradio git checkout signal_source_phase mkdir build && cd build cmake -DENABLE_INTERNAL_VOLK:BOOL=OFF -DENABLE_GR_FEC:BOOL=OFF -DENABLE_GR_DIGITAL:BOOL=OFF -DENABLE_GR_DTV:BOOL=OFF -DENABLE_GR_ATSC:BOOL=OFF -DENABLE_GR_AUDIO:BOOL=OFF -DENABLE_GR_CHANNELS:BOOL=OFF -DENABLE_GR_NOAA:BOOL=OFF -DENABLE_GR_PAGER:BOOL=OFF -DENABLE_GR_TRELLIS:BOOL=OFF -DENABLE_GR_VOCODER:BOOL=OFF .. make sudo make install
Build and install libsigrok
cd ~ git clone https://github.com/sigrokproject/libsigrok/ mkdir -p libsigrok/build cd libsigrok/build ../autogen.sh ../configure --disable-all-drivers --enable-bindings --enable-cxx make -j4 install
Build and install libsigrokdecode
cd ~ mkdir -p libsigrokdecode-0.4.1/build wget http://sigrok.org/download/source/libsigrokdecode/libsigrokdecode-0.4.1.tar.gz tar -xzvf libsigrokdecode-0.4.1.tar.gz cd libsigrokdecode-0.4.1/build ../configure --enable-shared --disable-static make -j4 install
Build and install Qwt
Before building Qwt, you need to check out your version of qmake.
Please make sure you are using Qt 5. For the next steps, use the full path to qmake.
Now we can build and install Qwt:
cd ~ git clone https://github.com/osakared/qwt -b qwt-6.1-multiaxes cd qwt curl https://raw.githubusercontent.com/analogdevicesinc/scopy-snap/master/qwt-6.1-multiaxes.patch | patch -p1 # Use full path to qmake qmake qwt.pro make -j4 sudo make install
Build and install Qwt Polar
cd ~ curl -L https://downloads.sourceforge.net/project/qwtpolar/qwtpolar/1.1.1/qwtpolar-1.1.1.tar.bz2 | tar -xj cd qwtpolar-1.1.1 curl https://raw.githubusercontent.com/analogdevicesinc/scopy-snap/master/qwtpolar-qwt-6.1-compat.patch |patch -p1
Change QWT_POLAR_INSTALL_PREFIX to /usr/local and remove the following lines:
QWT_POLAR_CONFIG += QwtPolarExamples \\ QWT_POLAR_CONFIG += QwtPolarDesigner \\ QWT_POLAR_CONFIG += QwtPolarFramework \\ QWT_POLAR_INSTALL_FEATURES = $${QWT_POLAR_INSTALL_PREFIX}/features \\
After that, change QWT_POLAR_INSTALL_PREFIX to /usr/local and QWT_POLAR_INSTALL_HEADERS to $${QWT_POLAR_INSTALL_PREFIX}/include/qwt
# Use full path to qmake qmake LIBS+=“-L/usr/local/lib -lqwt” INCLUDEPATH+=“/usr/local/include/qwt” qwtpolar.pro make -j4 sudo make install
Install libad9361
cd ~ git clone https://github.com/analogdevicesinc/libad9361-iio cd libad9361-iio mkdir build && cd build cmake .. make sudo make install
Build and install the IIO blocks for GNU Radio
cd ~ git clone https://github.com/analogdevicesinc/gr-iio cd gr-iio mkdir build && cd build cmake .. make sudo make install
git clone https://github.com/analogdevicesinc/scopy.gitThis will fetch the latest sources from GitHub to a “scopy” directory.
cd scopy mkdir build && cd build cmake ..If everything goes well, the output should be “Configuring done” and “Generating done”.
Now build the project:
makeAnd run Scopy:
./scopy
Return to Scopy Main Page