Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
university:tools:m2k:libm2k:calibration [22 Oct 2020 15:33] Adrian Suciuuniversity:tools:m2k:libm2k:calibration [04 May 2021 07:41] (current) – add temp file max size Alexandra Trifan
Line 29: Line 29:
 ==== Generating the file ==== ==== Generating the file ====
 The calibration values are written to the context attribute from a file on the ADALM2000 partition. The values will be stored on the device until they are overwritten. The calibration values are written to the context attribute from a file on the ADALM2000 partition. The values will be stored on the device until they are overwritten.
 +
 +<note important> There is a known limitation: The maximum temperature file size is 4 kb. This will change in a future release. </note>
  
 This file must be called 'm2k-calib-temp-lut.ini' and it should contain only a row having the following format: This file must be called 'm2k-calib-temp-lut.ini' and it should contain only a row having the following format:
university/tools/m2k/libm2k/calibration.txt · Last modified: 04 May 2021 07:41 by Alexandra Trifan