This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:m2k:accessories:power [23 Jul 2021 14:48] – [Getting started] Pop Andreea | university:tools:m2k:accessories:power [05 May 2022 12:44] (current) – Update pics Pop Andreea | ||
---|---|---|---|
Line 3: | Line 3: | ||
The AD-M2KPWR-EBZ is an ADALM2000 add-on board which increases the output current capability up to 700mA. This board can be also used as a standalone benchtop power supply with positive and negative outputs. | The AD-M2KPWR-EBZ is an ADALM2000 add-on board which increases the output current capability up to 700mA. This board can be also used as a standalone benchtop power supply with positive and negative outputs. | ||
- | {{: | + | {{: |
+ | {{: | ||
- | Figure 1. AD-M2KPWR-EBZ Top view | + | |
+ | Figure 1. AD-M2KPWR-EBZ Top view and bottom | ||
===== Features ===== | ===== Features ===== | ||
* ADALM2000 compatible | * ADALM2000 compatible | ||
Line 26: | Line 28: | ||
* 0V to 5V (400mA in USB power mode) | * 0V to 5V (400mA in USB power mode) | ||
* -5V to 0V (400mA in USB power mode) | * -5V to 0V (400mA in USB power mode) | ||
- | - Two variable power supplies, | + | - Two |
* 1.5V to 15V (up to 700mA if powered with 18V) | * 1.5V to 15V (up to 700mA if powered with 18V) | ||
Line 40: | Line 42: | ||
* Standoffs and screws | * Standoffs and screws | ||
- | {{: | + | {{: |
Figure 2. AD-M2KPWR-EBZ Isometric view - Package contents | Figure 2. AD-M2KPWR-EBZ Isometric view - Package contents | ||
Line 46: | Line 49: | ||
AD-M2KPWR-EBZ | AD-M2KPWR-EBZ | ||
+ | <WRAP centeralign> | ||
+ | <WRAP centeralign> | ||
+ | ^ P2 ^ Selected supply method^ | ||
+ | |Jumper 1-2 shorted | Vext - for external lab supply| | ||
+ | |Jumper 2-3 shorted | Vusb - for USB Type C power adapter| | ||
- | {{: | ||
- | Vext - for external lab supply | ||
- | Vusb - for USB Type C power adapter | + | <WRAP centeralign> |
- | The board has two modes: | + | ====M2K and POT modes ==== |
In M2K mode the board is plugged into ADALM2000. After that, the programable user supplies of ADALM2000 can be used as usual, but they will source more current. The jumper on the connector P7 must be in M2K- position and the jumper on the connector P6 must be in M2K+ position. | In M2K mode the board is plugged into ADALM2000. After that, the programable user supplies of ADALM2000 can be used as usual, but they will source more current. The jumper on the connector P7 must be in M2K- position and the jumper on the connector P6 must be in M2K+ position. | ||
- | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
+ | <WRAP centeralign> | ||
+ | |||
+ | |||
+ | ^ P6 ^ Output voltage ^ ^ | ||
+ | |Jumper 1-2 shorted | Positive supply adjusted by R20 |( 1.5 -> 15V)| | ||
+ | |Jumper 2-3 shorted | Positive supply of M2K |( 0V-> 5V)| | ||
+ | |||
+ | ^ P7 ^ Output voltage ^ ^ | ||
+ | |Jumper 1-2 shorted | Negative supply adjusted by R19 | ( -15V -> -1.5V )| | ||
+ | |Jumper 2-3 shorted | Negative supply of M2K | ( -5V -> 0V)| | ||
+ | |||
In POT mode the board can be used as a standalone benchtop power supply. The output voltage is adjusted with potentiometers R19 and R20. The output voltage will be available at the same pins: V+ and V-. | In POT mode the board can be used as a standalone benchtop power supply. The output voltage is adjusted with potentiometers R19 and R20. The output voltage will be available at the same pins: V+ and V-. | ||
- | <WRAP centeralign> | + | |
- | <WRAP centeralign> | + | ====Gain==== |
+ | The board can be adjusted such as the output voltage is double or triple than the value set from the M2K. This feature is only available in M2K mode, and it is activated by soldering or desoldering the solderjumpers on the bottom of the board according to the table. | ||
+ | You can find the table with the soldering instructions on the bottom of the board. | ||