This is an old revision of the document!
The AD-M2KPWR-EBZ is and ADALM2000 add-on board which increases the output current capability up to 700mA. This board can be also used as a standalone benchtop power supply with positive and negative outputs.
Figure 1. AD-M2KPWR-EBZ Top view
The AD-M2KPWR-EBZ is a USB Type C powered board capable to increase the output current of ADALM2000’s power supplies.
Inputs:
Switching between the inputs is done with a jumper.
Outputs: (2 control modes)
AD-M2KPWR-EBZ and must be supplied either from a 5.1V 3A USB Type C power adapter or from a lab supply using the screw terminal connector. Make sure that the jumper on the P2 connector is on the position corresponding to the chosen supply:
Vext - for external lab supply Vusb - for USB Type C power adapter
The board has two modes: M2K and POT
In M2K mode the board is plugged into ADALM2000. After that, the programable user supplies of ADALM2000 can be used as usual, but they will source more current. The jumper on the connector P7 must be in M2K- position and the jumper on the connector P6 must be in M2K+ position.
Figure 3. AD-M2KPWR-EBZ connected to ADALM2000 and USB Type C supply
In POT mode the board can be used as a standalone benchtop power supply. The output voltage is adjusted with potentiometers R19 and R20.
Figure 4. AD-M2KPWR-EBZ POT mode setup