This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:tools:m2k:accessories:power [27 Aug 2021 14:01] – Replaced pictures Pop Andreea | university:tools:m2k:accessories:power [18 Mar 2022 15:38] – Gains Pop Andreea | ||
---|---|---|---|
Line 3: | Line 3: | ||
The AD-M2KPWR-EBZ is an ADALM2000 add-on board which increases the output current capability up to 700mA. This board can be also used as a standalone benchtop power supply with positive and negative outputs. | The AD-M2KPWR-EBZ is an ADALM2000 add-on board which increases the output current capability up to 700mA. This board can be also used as a standalone benchtop power supply with positive and negative outputs. | ||
+ | {{: | ||
+ | {{: | ||
- | {{: | ||
- | {{: | ||
Figure 1. AD-M2KPWR-EBZ Top view and bottom view | Figure 1. AD-M2KPWR-EBZ Top view and bottom view | ||
Line 42: | Line 42: | ||
* Standoffs and screws | * Standoffs and screws | ||
+ | {{: | ||
- | {{: | ||
Line 50: | Line 50: | ||
AD-M2KPWR-EBZ | AD-M2KPWR-EBZ | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
<WRAP centeralign> | <WRAP centeralign> | ||
^ P2 ^ Selected supply method^ | ^ P2 ^ Selected supply method^ | ||
Line 58: | Line 58: | ||
- | <WRAP centeralign> | + | |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 66: | Line 66: | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 82: | Line 82: | ||
+ | ====Gain==== | ||
+ | The board can be adjusted such as the output voltage is double or triple than the value set from the M2K. This feature is only available in M2K mode, and it is activated by soldering or desoldering the solderjumpers on the bottom of the board according to the table. | ||
+ | You can find the table with the soldering instructions on the bottom of the board. | ||