This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:tools:m2k:accessories:power [23 Jul 2021 15:19] – [Description] Pop Andreea | university:tools:m2k:accessories:power [27 Jul 2021 09:25] – Edited pictures Pop Andreea | ||
---|---|---|---|
Line 46: | Line 46: | ||
AD-M2KPWR-EBZ | AD-M2KPWR-EBZ | ||
- | + | <WRAP centeralign> | |
- | {{: | + | <WRAP centeralign> |
^ P2 ^ Selected supply method^ | ^ P2 ^ Selected supply method^ | ||
|Jumper 1-2 shorted | Vext - for external lab supply| | |Jumper 1-2 shorted | Vext - for external lab supply| | ||
|Jumper 2-3 shorted | Vusb - for USB Type C power adapter| | |Jumper 2-3 shorted | Vusb - for USB Type C power adapter| | ||
+ | |||
+ | |||
+ | <WRAP centeralign> | ||
+ | <WRAP centeralign> | ||
====M2K and POT modes ==== | ====M2K and POT modes ==== | ||
Line 58: | Line 61: | ||
In M2K mode the board is plugged into ADALM2000. After that, the programable user supplies of ADALM2000 can be used as usual, but they will source more current. The jumper on the connector P7 must be in M2K- position and the jumper on the connector P6 must be in M2K+ position. | In M2K mode the board is plugged into ADALM2000. After that, the programable user supplies of ADALM2000 can be used as usual, but they will source more current. The jumper on the connector P7 must be in M2K- position and the jumper on the connector P6 must be in M2K+ position. | ||
- | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
+ | <WRAP centeralign> | ||
Line 74: | Line 77: | ||
In POT mode the board can be used as a standalone benchtop power supply. The output voltage is adjusted with potentiometers R19 and R20. The output voltage will be available at the same pins: V+ and V-. | In POT mode the board can be used as a standalone benchtop power supply. The output voltage is adjusted with potentiometers R19 and R20. The output voltage will be available at the same pins: V+ and V-. | ||
- | <WRAP centeralign> | + | |
- | <WRAP centeralign> | + | |