This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:m1k:firmware-upgrade [01 Mar 2018 10:36] – Add a troubleshooting section and remove the manual upgrade section for now. Alexandra Trifan | university:tools:m1k:firmware-upgrade [08 Feb 2021 16:58] (current) – update links to libsmu wiki page Alexandra Trifan | ||
---|---|---|---|
Line 1: | Line 1: | ||
===== ADALM1000 Firmware Upgrade Procedures ===== | ===== ADALM1000 Firmware Upgrade Procedures ===== | ||
- | The firmware on the device can be upgraded directly from Pixelpulse. | + | The firmware on the device can be upgraded |
+ | |||
+ | ==== Update using the smu executable ==== | ||
+ | |||
+ | The '' | ||
+ | <WRAP box bggreen>< | ||
+ | < | ||
+ | C: | ||
+ | smu: utility for managing M1K devices | ||
+ | |||
+ | -h, --help | ||
+ | | ||
+ | -l, --list-devices | ||
+ | -p, --hotplug-devices | ||
+ | -s, --stream-samples | ||
+ | -d, --display-calibration | ||
+ | -r, --reset-calibration | ||
+ | -w, --write-calibration <cal file> write calibration data to a single attached device | ||
+ | -f, --flash < | ||
+ | </ | ||
+ | </ | ||
+ | |||
+ | As you can see in the above, the '' | ||
+ | |||
+ | After downloading the firmware binary, run the following command in your OS specific preferred terminal: | ||
+ | < | ||
+ | C: | ||
+ | </ | ||
+ | |||
+ | After installing '' | ||
==== Automatic update from Pixelpulse ==== | ==== Automatic update from Pixelpulse ==== |