This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:m1k:calibration [08 Feb 2021 16:55] – update links to libsmu wiki page Alexandra Trifan | university:tools:m1k:calibration [09 Feb 2021 15:19] (current) – [ADALM1000 Calibration Procedure] Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== ADALM1000 Calibration Procedure ====== | ====== ADALM1000 Calibration Procedure ====== | ||
+ | |||
+ | <WRAP important> | ||
+ | Note that Revision F of the M1k is calibrated in the Factory and does not need the user to perform any calibration. The purpose of this Document is codify the steps required if the factory settings need to be changed or updated and for the legacy Revision D of the M1k hardware. | ||
+ | </ | ||
The ADALM1000 device can be calibrated by the user to achieve more accurate measurements and signal generation. The calibration procedure requires a Digital Multimeter (DMM) and a resistor with a value anywhere between 2.5Ω and 25Ω. | The ADALM1000 device can be calibrated by the user to achieve more accurate measurements and signal generation. The calibration procedure requires a Digital Multimeter (DMM) and a resistor with a value anywhere between 2.5Ω and 25Ω. | ||
Line 174: | Line 178: | ||
=====Semi-automated Procedure===== | =====Semi-automated Procedure===== | ||
- | + | The [[:university: | |
- | The [[university: | + |