This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:tools:m1k:calibration [26 Mar 2016 00:49] – Tim Harder | university:tools:m1k:calibration [09 Feb 2021 15:15] – [Semi-automated Procedure] Doug Mercer | ||
---|---|---|---|
Line 74: | Line 74: | ||
<WRAP round download 60%> | <WRAP round download 60%> | ||
- | {{https:// | + | {{https:// |
</ | </ | ||
Line 88: | Line 88: | ||
===== Storing the calibration data into the device ===== | ===== Storing the calibration data into the device ===== | ||
- | There are two methods to store the calibration data into the device: | + | To store the calibration data into the device: |
- | * Use the //smu// binary by typing in a terminal //smu --calibrate | + | * Use the //smu// binary by typing in a terminal //smu --write-calibration |
- | * Use the calibrate python script in the examples directory for the libsmu python bindings (or manually use the support via the python bindings). | + | |
The smu binary also supports displaying and resetting calibration for all supported, attached devices via the following: | The smu binary also supports displaying and resetting calibration for all supported, attached devices via the following: | ||
- | * resetting: //smu --reset-calibration// | + | * reset: //smu --reset-calibration// |
- | * displaying: //smu --display-calibration// | + | * display: //smu --display-calibration// |
- | To acquire the smu binary, use the libsmu installer below in addition to installing the correct architecture support for Microsoft' | + | <WRAP round important 60%> |
+ | Make sure that Pixelpulse is closed when running the //smu// binary. | ||
+ | </ | ||
+ | |||
+ | To acquire the smu binary, use the libsmu installer below in addition to installing the correct architecture support for Microsoft' | ||
+ | |||
+ | Instructions on how to build, install and use libsmu can be found [[university: | ||
<WRAP round download 60%> | <WRAP round download 60%> | ||
- | libsmu installer: [[https://ci.appveyor.com/ | + | libsmu installer: [[https://github.com/ |
</ | </ | ||
Line 167: | Line 172: | ||
* Read the current measurement on the DMM | * Read the current measurement on the DMM | ||
* Replace into the calibration file in the //**# Channel A/B, source I**// sections the //< -0.1000, -0.1000>// | * Replace into the calibration file in the //**# Channel A/B, source I**// sections the //< -0.1000, -0.1000>// | ||
+ | |||
+ | =====Semi-automated Procedure===== | ||
+ | The [[: |