This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:tools:m1k:analog-mux [29 Dec 2020 19:23] – new analog accessory board version Doug Mercer | university:tools:m1k:analog-mux [30 Dec 2020 17:17] – add sparkfun links Doug Mercer | ||
---|---|---|---|
Line 44: | Line 44: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
+ | There are other analog multiplexer configurations in the generic CD4XXX series of CMOS ICs. The CD4051 is a single 8:1 mux and the CD4067 is a single 16:1 mux. The old Motorola MC14529B analog selector can be a configured as a dual 4-channel or single 8-channel device depending on how the input controls are used. By using 3 or all 4 of the digital PIO bits and two of these single multiplexers either 16 or even 32 signal channels could be measured. This [[https:// | ||
The SparkFun analog mux boards do not come with header connectors so they would need to be added. The pins on the connector do not line up with the M1k connectors so male to male jumpers would be needed as shown in the figure 9. | The SparkFun analog mux boards do not come with header connectors so they would need to be added. The pins on the connector do not line up with the M1k connectors so male to male jumpers would be needed as shown in the figure 9. |