This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:tools:m1k:analog-mux [25 Mar 2016 18:15] – ↷ Links adapted because of a move operation Robin Getz | university:tools:m1k:analog-mux [19 Aug 2016 20:17] – add 74HC4051 based bob Doug Mercer | ||
---|---|---|---|
Line 33: | Line 33: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | There are other analog multiplexer configurations in the generic CD4XXX series of CMOS ICs. The CD4051 is a single 8:1 mux and the CD4067 is a single 16:1 mux. The old Motorola MC14529B analog selector can be a configured as a dual 4-channel or single 8-channel device depending on how the input controls are used. By using 3 or all 4 of the digital PIO bits and two of these single multiplexers either 16 or even 32 signal channels could be measured. | + | There are other analog multiplexer configurations in the generic CD4XXX series of CMOS ICs. The CD4051 is a single 8:1 mux and the CD4067 is a single 16:1 mux. The old Motorola MC14529B analog selector can be a configured as a dual 4-channel or single 8-channel device depending on how the input controls are used. By using 3 or all 4 of the digital PIO bits and two of these single multiplexers either 16 or even 32 signal channels could be measured. |
Another functionally similar option is the [[http:// | Another functionally similar option is the [[http:// |