Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:tools:m1k:analog-mux [08 Apr 2022 19:58]
Doug Mercer add MAX4618 and MAX4582 as options
university:tools:m1k:analog-mux [21 Dec 2022 18:49]
Doug Mercer fix a couple of things
Line 71: Line 71:
 The TTL compatible digital input minimum logic high voltage spec for the ADG609 is 2.45 V where the CD4052 and 74HC4052 minimum logic high voltage spec is 3.15V which is just slightly lower than the 3.3V typical logic high output voltage generated by the ALM1000. The actual logic threshold for the CD4052 is probably closer to VDD/2 ( 2.5V ) at room temperature and seems to work ( given this will probably be used at room temperature ) but there could be little margin in certain cases. The TTL compatible 74HCT4052 has a 1.6 volt typical logic high threshold which is perfect for the 3.3 V CMOS outputs of the ALM1000. The TTL compatible digital input minimum logic high voltage spec for the ADG609 is 2.45 V where the CD4052 and 74HC4052 minimum logic high voltage spec is 3.15V which is just slightly lower than the 3.3V typical logic high output voltage generated by the ALM1000. The actual logic threshold for the CD4052 is probably closer to VDD/2 ( 2.5V ) at room temperature and seems to work ( given this will probably be used at room temperature ) but there could be little margin in certain cases. The TTL compatible 74HCT4052 has a 1.6 volt typical logic high threshold which is perfect for the 3.3 V CMOS outputs of the ALM1000.
  
-This analog multiplexer data acquisition add-on board is a perfect candidate for writing a custom program using the ALM1000 Python interface software package ([[https://​github.com/​signalspec/​libsmu|libpysmu]]). A basic example Python program (eight-channel-mux.py) is written with a minimal display but provides all the ALM1000 ​libpysmu ​specific code to pole the dual 4:1 MUX inputs through the two analog input channels A and B. The display window as shown in figure 11 displays the 8 raw voltage values. The program can of course be further customized by the user to display the input signals in the appropriate scale factor with any gain and offset calibration for the sensor(s) being used. A copy of the Python program is included in the zip file.+This analog multiplexer data acquisition add-on board is a perfect candidate for writing a custom program using the ALM1000 Python interface software package ([[https://​github.com/​signalspec/​libsmu|pysmu]]). A basic example Python program (eight-channel-mux.py) is written with a minimal display but provides all the ALM1000 ​pysmu specific code to pole the dual 4:1 MUX inputs through the two analog input channels A and B. The display window as shown in figure 11 displays the 8 raw voltage values. The program can of course be further customized by the user to display the input signals in the appropriate scale factor with any gain and offset calibration for the sensor(s) being used. A copy of the Python program is included in the zip file.
  
 {{ :​university:​tools:​m1k-analog-mux_f5.png?​300 |}} {{ :​university:​tools:​m1k-analog-mux_f5.png?​300 |}}
university/tools/m1k/analog-mux.txt · Last modified: 21 Dec 2022 18:49 by Doug Mercer