This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:alice-vvm-1.0-users-guide [14 Dec 2015 21:44] – [Main Graphics area] Doug Mercer | university:tools:m1k:alice:vvm-users-guide [27 Jan 2021 23:01] (current) – use interwiki links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
======ALICE Vector Voltmeter - Impedance Analyzer - RLC Meter: | ======ALICE Vector Voltmeter - Impedance Analyzer - RLC Meter: | ||
+ | |||
+ | **This software uses an older version of libsmu / pysmu and is no longer recommended for use.** | ||
+ | |||
+ | [[university: | ||
+ | |||
=====Objective: | =====Objective: | ||
Line 14: | Line 19: | ||
Windows:\\ | Windows:\\ | ||
- | [[https:// | + | [[https:// |
+ | |||
+ | Use of the [[university: | ||
Linux:\\ | Linux:\\ | ||
Line 93: | Line 100: | ||
[[university: | [[university: | ||
[[university: | [[university: | ||
- | [[university: | + | [[university: |
- | [[university: | + | [[university: |
- | [[university: | + | [[university: |
=====Making Measurements: | =====Making Measurements: | ||
Line 170: | Line 177: | ||
At the bottom of this section, just above the ADI logo, are entry windows which allow input gain and offset calibration to be added to the channel A and B inputs. For more on the use of input attenuators please refer to the following two documents: | At the bottom of this section, just above the ADI logo, are entry windows which allow input gain and offset calibration to be added to the channel A and B inputs. For more on the use of input attenuators please refer to the following two documents: | ||
- | [[university: | + | [[university: |
- | [[university: | + | [[university: |
=====Examples: | =====Examples: |