This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:alice-vvm-1.0-users-guide [14 Dec 2015 21:29] – [Directions:] Doug Mercer | university:tools:m1k:alice:vvm-users-guide [27 Jan 2021 23:01] (current) – use interwiki links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
======ALICE Vector Voltmeter - Impedance Analyzer - RLC Meter: | ======ALICE Vector Voltmeter - Impedance Analyzer - RLC Meter: | ||
+ | |||
+ | **This software uses an older version of libsmu / pysmu and is no longer recommended for use.** | ||
+ | |||
+ | [[university: | ||
+ | |||
=====Objective: | =====Objective: | ||
Line 14: | Line 19: | ||
Windows:\\ | Windows:\\ | ||
- | [[https:// | + | [[https:// |
+ | |||
+ | Use of the [[university: | ||
Linux:\\ | Linux:\\ | ||
Line 93: | Line 100: | ||
[[university: | [[university: | ||
[[university: | [[university: | ||
- | [[university: | + | [[university: |
- | [[university: | + | [[university: |
- | [[university: | + | [[university: |
=====Making Measurements: | =====Making Measurements: | ||
Line 133: | Line 140: | ||
The main graphics area is where the measured results are displayed. The impedance magnitude and angle along with the real and imaginary parts are drawn on the polar ( circular ) grid in Ohms. The real, series resistance component is drawn in green at 0 degrees phase. The imaginary part of the series impedance is drawn in red at either +90 degrees or -90 degrees depending on the sign. A positive impedance is inductive and an negative impedance is capacitive. The combined magnitude of the total series impedance is drawn in orange and at the measured angle. | The main graphics area is where the measured results are displayed. The impedance magnitude and angle along with the real and imaginary parts are drawn on the polar ( circular ) grid in Ohms. The real, series resistance component is drawn in green at 0 degrees phase. The imaginary part of the series impedance is drawn in red at either +90 degrees or -90 degrees depending on the sign. A positive impedance is inductive and an negative impedance is capacitive. The combined magnitude of the total series impedance is drawn in orange and at the measured angle. | ||
- | To the left of the grid the relative gain of Channel B to Channel A is displayed in dB. Next the relative phase is displayed in degrees. Next the measured frequency in Hz is displayed. Next the measured Impedance Magnitude, Angle, R series and X series are displayed. Finally the calculated capacitance ( if X series is negative ) or inductance ( if X series is positive ) is displayed. | + | To the right of the grid, the relative gain of Channel B to Channel A is displayed in dB. Next the relative phase is displayed in degrees. Next the measured frequency in Hz is displayed. Next the measured Impedance Magnitude, Angle, R series and X series are displayed. Finally the calculated capacitance ( if X series is negative ) or inductance ( if X series is positive ) is displayed. |
To convert the series values to the equivalent parallel values see Appendix A. | To convert the series values to the equivalent parallel values see Appendix A. | ||
Line 170: | Line 177: | ||
At the bottom of this section, just above the ADI logo, are entry windows which allow input gain and offset calibration to be added to the channel A and B inputs. For more on the use of input attenuators please refer to the following two documents: | At the bottom of this section, just above the ADI logo, are entry windows which allow input gain and offset calibration to be added to the channel A and B inputs. For more on the use of input attenuators please refer to the following two documents: | ||
- | [[university: | + | [[university: |
- | [[university: | + | [[university: |
=====Examples: | =====Examples: | ||
Line 205: | Line 212: | ||
====Example 2:==== | ====Example 2:==== | ||
- | We can use ALICE-VVM to measure the input capacitance of channel B. We know that the input capacitance is small so we will need to use a large value for R< | + | We can use ALICE-VVM to measure the input capacitance of channel B. We know that the input capacitance is small so we will need to use a large value for R< |
{{ : | {{ : |