This shows you the differences between two versions of the page.
Next revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:alice-sa-1.0-users-guide [03 Aug 2015 16:47] – created Doug Mercer | university:tools:alice-sa-1.0-users-guide [11 Aug 2015 02:30] – [Curves drop down menu] Doug Mercer | ||
---|---|---|---|
Line 56: | Line 56: | ||
In Average mode, the trace values are averaged. This smooths out the randomness in the noise floor. | In Average mode, the trace values are averaged. This smooths out the randomness in the noise floor. | ||
+ | In Single Shot mode a single sweep is obtained each time the Run button is pressed. | ||
====FFT window drop down menu==== | ====FFT window drop down menu==== | ||
Line 66: | Line 67: | ||
====Curves drop down menu==== | ====Curves drop down menu==== | ||
- | The Curves button allows the selection of which signal waveforms will be displayed. The All button selects all four curves to be displayed and the None button clears all four curves. The Marker option turns on a text marker which displays the amplitude and frequency at the peak of the displayed signal. It is also possible to select which of the possible stored reference traces, if saved via the Store trace option, will be displayed. | + | The Curves button allows the selection of which signal waveforms will be displayed. The All button selects all four curves to be displayed and the None button clears all four curves. The Marker option turns on a text marker which displays the amplitude and frequency at the peak of the displayed signal. Options to display the difference ( subtraction ) of the CA-V – CB-V traces or the CB-V – CA-V traces. It is also possible to select which of the possible stored reference traces, if saved via the Store trace option, will be displayed. |
====Run, Stop, Exit==== | ====Run, Stop, Exit==== |