This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:m1k:alice:oscilloscope-x-y-user-guide [27 Jan 2021 22:37] – use wp> interwiki links Robin Getz | university:tools:m1k:alice:oscilloscope-x-y-user-guide [25 Jun 2021 19:34] – [The Top Menu Section] Doug Mercer | ||
---|---|---|---|
Line 12: | Line 12: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
+ | ====The Top Menu Section==== | ||
+ | |||
+ | The menu section along the top, shown in figure 1T, contains various buttons and drop-down menus that control Oscilloscope Triggering, Horizontal time base, Horizontal position, how and what signals are displayed, and run acquisition looping / stop acquisition looping / exit program. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ===Triggering functions=== | ||
+ | |||
+ | The ADALM1000 signal generation and measurement hardware is tightly integrated and can operate in two modes. As an integrated Source/ | ||
+ | |||
+ | The Trigger button is a drop down menu listing which signal to trigger on, CA-V, CA-I, CB-V, CB-I or none. The use of Triggering to display a stable trace is generally necessary when viewing externally generated signals. When viewings internally generated signals from one or the other of the AWG channels a stable trace happens automatically when the AWG Sync function is enabled i.e. the beginning of the AWG output waveform is restarted at the same point at the start of each time sweep. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The Auto Level option automatically sets the trigger level to the selected waveform midpoint on each sweep. The trigger point will thus track any changes in the input waveform. | ||
+ | |||
+ | The Low Pass Filter option applies a variable length digital low pass filter function to the selected waveform before searching for the trigger condition. This can be used to filter high frequency noise that might be on the signal of interest and better stabilize the triggering. The length of the filter, in samples, can be set/ | ||
+ | |||
+ | When Manual Triggering is selected one sweep is acquired and displayed each time the green Run button is clicked. | ||
+ | |||
+ | When Single Shot Triggering is selected triggering is " | ||
+ | |||
+ | The Edge button is a drop down menu listing either the rising or falling edge for triggering. The Trigger Level entry window contains the trigger level in volts for CA-V and CB-V or mA for CA-I and CB-I. | ||
+ | |||
+ | The 50% button sets the trigger level to the midpoint (50% point) of the selected trigger waveform. i.e. to the (maximum + minimum)/2. | ||
+ | |||
+ | ===Horizontal Time Controls=== | ||
+ | |||
+ | < | ||
+ | |||
+ | There are two sweeping modes in the time domain display. The conventional time per Div based view and a rolling mode. The Roll Mode in a digital storage oscilloscope uses a display different from that of the usual time-based view. While viewing a very low-frequency periodic signal in the usual time per Div based view the screen up dates, is redrawn, with the next new trace only after a screen’s worth of data samples are captured. This can take a few seconds for 100 mS/Div or greater time bases. Rather, in Roll Mode the trace is redrawn continuously and moves from right to left along the time-axis as new samples are taken, resembling what you would see in an analog strip chart. The time axis, rather than starting at the triggering point as in conventional mode, remains static and the waveform moves or rolls. Accordingly, | ||
+ | |||
+ | The Hold Off entry window, in mS, is used to shift the horizontal position ( apparent time 0 start point ) within the acquired sample point buffers being displayed. The data used for the vertical and horizontal waveform calculations is also shifted by that amount. The sample buffer is generally two screens long so setting the hold off time to more than one screen width is not recommended. This is mainly used when synced to the AWG. Due to the discontinuous nature of the AWG outputs this allows the user to skip over any initial transients that might appear if the system being measured has " | ||
+ | |||
+ | The Horz Pos entry window is used to change the horizontal position of the time trace. Normally, with the Horz Pos set to 0 the left edge of the grid is "time 0". Setting Horz Pos to something else shifts the 0 time point on the grid by that amount ( in mSec ). So if you set Horz Poss to a negative number for example you can see time before the trigger. | ||
+ | |||
+ | The Time mS/Div spinbox entry window is used to set the horizontal time base in the standard 1, 2, 5 step increments. Other values maybe entered manually. | ||
+ | |||
+ | ===Trace Controls=== | ||
+ | |||
+ | The Curves drop down menu button allows the selection of which signal waveform traces will be displayed vs time. The All button selects all four curves to be displayed and the None button clears all four curves. Plot the Math-X and Math-Y formulas by clicking on those options. ALICE can automatically adjust the trace vertical position to center the CA-V and /or CB-V traces on the midpoint of the waveform each sweep by clicking on either or both of the options below the –Auto Vert Center- heading. | ||
+ | |||
+ | When using external Resistor Divider attenuators the frequency response of the Channel may be reduced. The software High Pass frequency compensation can be selected for either channel by clicking on the buttons below the –Input HP Comp- heading. See the section on Analog Inputs below | ||
+ | |||
+ | It is also possible to select which of the possible stored reference time traces, if saved via the Snap-Shot option, will be displayed. | ||
+ | |||
+ | At the bottom are options to enable the vertical Time and horizontal Voltage (Current) cursors. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The green PWR-On button toggles on and off the fixed analog +2.5 V and +5 V power supplies. The button turns red when the supplies are off. The power supplies do not turn completely off but go to around +2 V and can supply only about 20 mA when shorted to ground. This is much less than the 200 mA or so they could supply if accidentally shorted when on. It is good practice to turn off the supplies ( or better yet disconnect them ) when making any modifications to the circuit under test. | ||
+ | |||
+ | The green Run button starts continuous looping acquiring input samples. The red Stop button stops or pauses the acquisition looping. The Stop button also serves as a sort of refresh button. If the Stop button is clicked when stopped the graphics display is redrawn using any new settings that might have changed but using the existing data buffers. The Exit button exits (kills) the program. | ||
Many of the drop down menus on the main oscilloscope screen and the screens for the other instruments include accelerator keys, indicated by () around the accelerator keyboard character next to the menu item. Typing one of these characters while the mouse cursor is inside the graphics drawing area will invoke that menu function. For example typing 1 or 2 will toggle on and off the CA-V and CB-V traces. | Many of the drop down menus on the main oscilloscope screen and the screens for the other instruments include accelerator keys, indicated by () around the accelerator keyboard character next to the menu item. Typing one of these characters while the mouse cursor is inside the graphics drawing area will invoke that menu function. For example typing 1 or 2 will toggle on and off the CA-V and CB-V traces. | ||
+ | |||
+ | ===ALICE Scope/AWG only option=== | ||
By setting to 1 the EnableScopeOnly = 1; option in the alice_init.ini file, the Oscilloscope and AWG controls can be combined in one window as shown in figure 1S. The controls all work as they do in the default two window configuration (See [[university: | By setting to 1 the EnableScopeOnly = 1; option in the alice_init.ini file, the Oscilloscope and AWG controls can be combined in one window as shown in figure 1S. The controls all work as they do in the default two window configuration (See [[university: | ||
Line 250: | Line 312: | ||
[[university: | [[university: | ||
[[university: | [[university: | ||
- | |||
- | ====The Top Menu Section==== | ||
- | |||
- | The menu section along the top contains various buttons and drop-down menus that control Oscilloscope Triggering, Horizontal time base, Horizontal position, how and what signals are displayed, and run acquisition looping / stop acquisition looping / exit program. | ||
- | |||
- | ===Triggering functions=== | ||
- | |||
- | The ADALM1000 signal generation and measurement hardware is tightly integrated and can operate in two modes. As an integrated Source/ | ||
- | |||
- | The Trigger button is a drop down menu listing which signal to trigger on, CA-V, CA-I, CB-V, CB-I or none. The use of Triggering to display a stable trace is generally necessary when viewing externally generated signals. When viewings internally generated signals from one or the other of the AWG channels a stable trace happens automatically when the AWG Sync function is enabled i.e. the beginning of the AWG output waveform is restarted at the same point at the start of each time sweep. | ||
- | |||
- | {{ : | ||
- | |||
- | <WRAP centeralign> | ||
- | |||
- | The Auto Level option automatically sets the trigger level to the selected waveform midpoint on each sweep. The trigger point will thus track any changes in the input waveform. | ||
- | |||
- | The Low Pass Filter option applies a variable length digital low pass filter function to the selected waveform before searching for the trigger condition. This can be used to filter high frequency noise that might be on the signal of interest and better stabilize the triggering. The length of the filter, in samples, can be set/ | ||
- | |||
- | When Manual Triggering is selected one sweep is acquired and displayed each time the green Run button is clicked. | ||
- | |||
- | When Single Shot Triggering is selected triggering is " | ||
- | |||
- | The Edge button is a drop down menu listing either the rising or falling edge for triggering. The Trigger Level entry window contains the trigger level in volts for CA-V and CB-V or mA for CA-I and CB-I. | ||
- | |||
- | The 50% button sets the trigger level to the midpoint (50% point) of the selected trigger waveform. i.e. to the (maximum + minimum)/2. | ||
- | |||
- | ===Horizontal Time Controls=== | ||
- | |||
- | The Hold Off entry window, in mS, is used to shift the horizontal position ( apparent time 0 start point ) within the acquired sample point buffers being displayed. The data used for the vertical and horizontal waveform calculations is also shifted by that amount. The sample buffer is generally two screens long so setting the hold off time to more than one screen width is not recommended. This is mainly used when synced to the AWG. Due to the discontinuous nature of the AWG outputs this allows the user to skip over any initial transients that might appear if the system being measured has " | ||
- | |||
- | The Horz Pos entry window is used to change the horizontal position of the time trace. Normally, with the Horz Pos set to 0 the left edge of the grid is "time 0". Setting Horz Pos to something else shifts the 0 time point on the grid by that amount ( in mSec ). So if you set Horz Poss to a negative number for example you can see time before the trigger. | ||
- | |||
- | The Time mS/Div spinbox entry window is used to set the horizontal time base in the standard 1, 2, 5 step increments. Other values maybe entered manually. | ||
- | |||
- | ===Trace Controls=== | ||
- | |||
- | The Curves button allows the selection of which signal waveforms will be displayed when plotting vs time. The All button selects all four curves to be displayed and the None button clears all four curves. It is also possible to select which of the possible stored reference time traces, if saved via the Snap-Shot option, will be displayed. | ||
- | |||
- | The green PWR-On button toggles on and off the fixed analog +2.5 V and +5 V power supplies. The button turns red when the supplies are off. The power supplies do not turn completely off but go to around +2 V and can supply only about 20 mA when shorted to ground. This is much less than the 200 mA or so they could supply if accidentally shorted when on. It is good practice to turn off the supplies ( or better yet disconnect them ) when making any modifications to the circuit under test. | ||
- | |||
- | The green Run button starts continuous looping acquiring input samples. The red Stop button stops or pauses the acquisition looping. The Stop button also serves as a sort of refresh button. If the Stop button is clicked when stopped the graphics display is redrawn using any new settings that might have changed but using the existing data buffers. The Exit button exits (kills) the program. | ||
====The Bottom Menu Section==== | ====The Bottom Menu Section==== |