This shows you the differences between two versions of the page.
Both sides previous revision Previous revision Next revision | Previous revision Next revision Both sides next revision | ||
university:tools:m1k:alice:oscilloscope-x-y-user-guide [14 Oct 2020 16:26] Doug Mercer [Oscilloscope / Main Window:] |
university:tools:m1k:alice:oscilloscope-x-y-user-guide [25 Jun 2021 16:29] Doug Mercer Add future Roll Mode info |
||
---|---|---|---|
Line 12: | Line 12: | ||
<WRAP centeralign>Figure 1, ALICE Desktop main Oscilloscope window</WRAP> | <WRAP centeralign>Figure 1, ALICE Desktop main Oscilloscope window</WRAP> | ||
+ | |||
+ | <note>Roll Feature Available in Fall 2021 release</note> | ||
+ | |||
+ | There are two sweeping modes in the time domain display. The conventional time per Div based view and a rolling mode. The Roll Mode in a digital storage oscilloscope uses a display different from that of the usual time-based view. While viewing a very low-frequency periodic signal in the usual time per Div based view the screen up dates, is redrawn, with the next new trace only after a screen’s worth of data samples are captured. This can take a few seconds for 100 mS/Div or greater time bases. Rather, in Roll Mode the trace is redrawn continuously and moves from right to left along the time-axis as new samples are taken, resembling what you would see in an analog strip chart. The time axis, rather than starting at the triggering point as in conventional mode, remains static and the waveform moves or rolls. Accordingly, in roll mode, the trace enters at the right of side of the display and travels in a stately fashion across the grid at a speed that is determined by how fast the computer can update (redraw) the display. This will vary from computer to computer based on the speed of the machine you are running the software on. The Roll-Off and Roll-On button between the Time base Entry and Curves Drop down Menu toggles between the Sweep Modes. | ||
Many of the drop down menus on the main oscilloscope screen and the screens for the other instruments include accelerator keys, indicated by () around the accelerator keyboard character next to the menu item. Typing one of these characters while the mouse cursor is inside the graphics drawing area will invoke that menu function. For example typing 1 or 2 will toggle on and off the CA-V and CB-V traces. | Many of the drop down menus on the main oscilloscope screen and the screens for the other instruments include accelerator keys, indicated by () around the accelerator keyboard character next to the menu item. Typing one of these characters while the mouse cursor is inside the graphics drawing area will invoke that menu function. For example typing 1 or 2 will toggle on and off the CA-V and CB-V traces. | ||
Line 204: | Line 208: | ||
It would be nice to not have to use a compensation capacitor, adjustable or otherwise. A digital (software) frequency compensation feature has been implemented in the ALICE 1.3 Desktop software package. | It would be nice to not have to use a compensation capacitor, adjustable or otherwise. A digital (software) frequency compensation feature has been implemented in the ALICE 1.3 Desktop software package. | ||
- | The software frequency compensation for each channel consists of a cascade of two adjustable [[https://en.wikipedia.org/wiki/High-pass_filter#Algorithmic_implementation|first order high pass filters]]. The time constant and the gain of each stage can be adjusted. Normal first order high pass filters do not pass DC so a DC gain of 1 path is added to the overall second order high pass software compensation filter. This structure is often called a shelving filter because of the shape of its frequency response. | + | The software frequency compensation for each channel consists of a cascade of two adjustable [[wp>High-pass_filter#Algorithmic_implementation|first order high pass filters]]. The time constant and the gain of each stage can be adjusted. Normal first order high pass filters do not pass DC so a DC gain of 1 path is added to the overall second order high pass software compensation filter. This structure is often called a shelving filter because of the shape of its frequency response. |
In figure In2 we show the new controls for the input compensation. To turn on and off the compensation for Channels A and B check boxes are added under the Curves drop down menu. Turning on compensation applies to both the Scope and Spectrum tools (time and frequency measurements). The filter time constant and gain settings can be set using new entry slots in the Settings Controls screen. The DC gain and offset adjust controls are unchanged. | In figure In2 we show the new controls for the input compensation. To turn on and off the compensation for Channels A and B check boxes are added under the Curves drop down menu. Turning on compensation applies to both the Scope and Spectrum tools (time and frequency measurements). The filter time constant and gain settings can be set using new entry slots in the Settings Controls screen. The DC gain and offset adjust controls are unchanged. | ||
Line 428: | Line 432: | ||
There is also a check button to display the saved X-Y reference trace (see note above in Oscilloscope section on Snap-Shot option). | There is also a check button to display the saved X-Y reference trace (see note above in Oscilloscope section on Snap-Shot option). | ||
+ | |||
+ | {{ :university:tools:m1k:alice:alice_xy-plot_lissajous_pattern.pdf |Using ALICE XY display and The Lissajous Pattern}} | ||
=====Oscilloscope and X-Y Plot Examples:===== | =====Oscilloscope and X-Y Plot Examples:===== |