This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:alm1000-meter-source-users-guide [25 Mar 2016 17:57] – ↷ Links adapted because of a move operation Robin Getz | university:tools:m1k:alice:meter-source-users-guide [27 Jan 2021 23:01] (current) – use interwiki links Robin Getz | ||
---|---|---|---|
Line 7: | Line 7: | ||
=====Background: | =====Background: | ||
- | The ALM1000 contains two 16 bit 100KSPS analog to digital converters and two 16 bit digital to analog converters. Along with a means to source both voltage and current with the DACs the system can simultaneously measure the current or voltage. These inputs and outputs are often used to measure time varying waveforms as in the [[university: | + | The ALM1000 contains two 16 bit 100KSPS analog to digital converters and two 16 bit digital to analog converters. Along with a means to source both voltage and current with the DACs the system can simultaneously measure the current or voltage. These inputs and outputs are often used to measure time varying waveforms as in the [[university: |
=====Required files:===== | =====Required files:===== | ||
Line 19: | Line 19: | ||
====Windows: | ====Windows: | ||
- | [[https://ci.appveyor.com/ | + | [[https:// |
Line 30: | Line 30: | ||
It is assumed that the reader is somewhat familiar with the functionality and capabilities of the ADALM1000 hardware. For more on the ADALM1000 hardware please refer to the following documents: | It is assumed that the reader is somewhat familiar with the functionality and capabilities of the ADALM1000 hardware. For more on the ADALM1000 hardware please refer to the following documents: | ||
- | [[university: | + | [[university: |
- | [[university: | + | [[university: |
[[university: | [[university: | ||
[[university: | [[university: |