This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:alm1000-meter-source-users-guide [02 Dec 2015 16:59] – [All OS:] Doug Mercer | university:tools:m1k:alice:meter-source-users-guide [27 Jan 2021 23:01] (current) – use interwiki links Robin Getz | ||
---|---|---|---|
Line 7: | Line 7: | ||
=====Background: | =====Background: | ||
- | The ALM1000 contains two 16 bit 100KSPS analog to digital converters and two 16 bit digital to analog converters. Along with a means to source both voltage and current with the DACs the system can simultaneously measure the current or voltage. These inputs and outputs are often used to measure time varying waveforms as in the [[university: | + | The ALM1000 contains two 16 bit 100KSPS analog to digital converters and two 16 bit digital to analog converters. Along with a means to source both voltage and current with the DACs the system can simultaneously measure the current or voltage. These inputs and outputs are often used to measure time varying waveforms as in the [[university: |
=====Required files:===== | =====Required files:===== | ||
Line 19: | Line 19: | ||
====Windows: | ====Windows: | ||
- | [[https:// | + | [[https:// |
====Linux: | ====Linux: | ||
Line 29: | Line 30: | ||
It is assumed that the reader is somewhat familiar with the functionality and capabilities of the ADALM1000 hardware. For more on the ADALM1000 hardware please refer to the following documents: | It is assumed that the reader is somewhat familiar with the functionality and capabilities of the ADALM1000 hardware. For more on the ADALM1000 hardware please refer to the following documents: | ||
- | [[university: | + | [[university: |
- | [[university: | + | [[university: |
- | [[university: | + | [[university: |
[[university: | [[university: | ||
[[university: | [[university: | ||
Line 63: | Line 64: | ||
=====Use Examples: | =====Use Examples: | ||
- | To demonstrate using the ALM1000 to measure current while sourcing voltage consider the resistor current divider circuit shown in figure E1. We would like to measure the currents flowing in resistors R< | + | To demonstrate using the ALM1000 to measure current while sourcing voltage consider the resistor current divider circuit shown in figure E1. We would like to measure the currents flowing in resistors R< |
{{ : | {{ : |