Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
university:tools:alm1000-meter-source-users-guide [25 Mar 2016 18:12] – ↷ Links adapted because of a move operation Robin Getzuniversity:tools:m1k:alice:meter-source-users-guide [27 Jan 2021 23:01] (current) – use interwiki links Robin Getz
Line 7: Line 7:
 =====Background:===== =====Background:=====
  
-The ALM1000 contains two 16 bit 100KSPS analog to digital converters and two 16 bit digital to analog converters. Along with a means to source both voltage and current with the DACs the system can simultaneously measure the current or voltage. These inputs and outputs are often used to measure time varying waveforms as in the [[university:tools:alice-1.0-users-guide|ALICE oscilloscope interface]]. However, there are often times when simple, accurate, DC measurements are required such as in a resistor network. The following Python interface is provided for that purpose. It provides the means to more accurately calibrate the measurements than provided by the factory calibration contained on the ALM1000 board itself.+The ALM1000 contains two 16 bit 100KSPS analog to digital converters and two 16 bit digital to analog converters. Along with a means to source both voltage and current with the DACs the system can simultaneously measure the current or voltage. These inputs and outputs are often used to measure time varying waveforms as in the [[university:tools:m1k:alice:users-guide|ALICE oscilloscope interface]]. However, there are often times when simple, accurate, DC measurements are required such as in a resistor network. The following Python interface is provided for that purpose. It provides the means to more accurately calibrate the measurements than provided by the factory calibration contained on the ALM1000 board itself.
  
 =====Required files:===== =====Required files:=====
Line 19: Line 19:
 ====Windows:==== ====Windows:====
  
-[[https://ci.appveyor.com/api/projects/analogdevicesinc/libsmu/artifacts/libpysmu.pyd?branch=master&job=Platform%3A%20x64|libpysmu.pyd (64 bit)]] [[https://ci.appveyor.com/api/projects/analogdevicesinc/libsmu/artifacts/libpysmu.pyd?branch=master&job=Platform%3A%20x86|libpysmu.pyd (32 bit)]] (needs to be in Python27\DLLs directory)+[[https://ci.appveyor.com/api/projects/analogdevicesinc/libsmu/artifacts/libpysmu.pyd?branch=master&job=Platform%3A%20x64|libpysmu.pyd (64 bit)]] [[https://ci.appveyor.com/api/projects/analogdevicesinc/libsmu/artifacts/libpysmu.pyd?branch=master&job=Platform%3A%20x86|libpysmu.pyd (32 bit)]] (needs to be in Python27\DLLs directory)
  
  
Line 31: Line 31:
  
 [[university:tools:m1k:alice:voltmeter-users-guide|ADALM1000 Voltmeter User's Guide]]\\ [[university:tools:m1k:alice:voltmeter-users-guide|ADALM1000 Voltmeter User's Guide]]\\
-[[university:tools:alm1000-ohmmeter-users-guide|ADALM1000 Ohmmeter User's Guide]]\\+[[university:tools:m1k:alice:ohmmeter-users-guide|ADALM1000 Ohmmeter User's Guide]]\\
 [[university:tools:m1k:analog-inputs|ADALM1000 Analog Inputs]] ( especially useful )\\ [[university:tools:m1k:analog-inputs|ADALM1000 Analog Inputs]] ( especially useful )\\
 [[university:tools:m1k|ADALM1000 Overview]]\\ [[university:tools:m1k|ADALM1000 Overview]]\\
university/tools/m1k/alice/meter-source-users-guide.txt · Last modified: 27 Jan 2021 23:01 by Robin Getz