This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:tools:m1k:alice:desktop-sa-ba-ia-users-guide [27 Jul 2020 19:42] – fix math formating Doug Mercer | university:tools:m1k:alice:desktop-sa-ba-ia-users-guide [20 Aug 2021 15:59] – [The menu buttons:] Doug Mercer | ||
---|---|---|---|
Line 80: | Line 80: | ||
The Angle for the Phase axis center can be set using this entry widget. | The Angle for the Phase axis center can be set using this entry widget. | ||
+ | |||
+ | **Vertical Axis Settings** | ||
+ | |||
+ | The vertical axis can display the signal amplitude in dBV (1 Vrms = 0 dB) or Vrms. When displaying in Vrms the scale can either linear or log. The signal can also be displayed as Power Spectral Density (PSD) in Vrms or dB per square-root-Hz. | ||
**dB/div +/- buttons** | **dB/div +/- buttons** | ||
Line 88: | Line 92: | ||
Used to set the top line of the grid or reference level. Sometimes called the " | Used to set the top line of the grid or reference level. Sometimes called the " | ||
+ | |||
=====The Bode Plotter: | =====The Bode Plotter: |